Hello community,
I have a question about MIPI DSI phy.
At first, our imx6solo board with mipi display himax8369 works well.
Now we have a mipi-display with himax8363 as the controler IC, and their FAE tells us the controller IC cannot run with too high mipi-clock signal, 150MHz at the maximum.
So when we try to change
static struct mipi_lcd_config lcd_config = {
.virtual_ch = 0x0,
.data_lane_num = HX8369_TWO_DATA_LANE, // HX8369_ONE_DATA_LANE
.max_phy_clk = HX8369_MAX_DPHY_CLK, // which is 800MHz
.dpi_fmt = MIPI_RGB888, /* original */
};
to the configuration below
static struct mipi_lcd_config lcd_config = {
.virtual_ch = 0x0,
.data_lane_num = HX8369_TWO_DATA_LANE, // HX8369_ONE_DATA_LANE
.max_phy_clk = 200,
.dpi_fmt = MIPI_RGB888, /* original */
};
there comes too many mipi dsi interrupts during the booting process after that change as follows,
mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver mipi_dsi
mxc_mipi_dsi mxc_mipi_dsi: dphy_pll_config:div 0x44.
mxc_mipi_dsi mxc_mipi_dsi: dphy_pll_config: i 20 max_phy_clk 200.
mxc_mipi_dsi mxc_mipi_dsi: MIPI DSI LCD setup.
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x6383ffb9
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x073081b1
mxc_mipi_dsi mxc_mipi_dsi: buf[1]=0x12070430
mxc_mipi_dsi mxc_mipi_dsi: buf[2]=0x003f423a
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x0000703a
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x000001b3
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x721208b4
mxc_mipi_dsi mxc_mipi_dsi: buf[1]=0x54030612
mxc_mipi_dsi mxc_mipi_dsi: buf[2]=0x00004e03
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x001000bf
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x00000eb6
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x000003cc
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x008000e0
mxc_mipi_dsi mxc_mipi_dsi: buf[1]=0x05a7138c
mxc_mipi_dsi mxc_mipi_dsi: buf[2]=0x17d4100d
mxc_mipi_dsi mxc_mipi_dsi: buf[3]=0x03071655
mxc_mipi_dsi mxc_mipi_dsi: buf[4]=0x8c008000
mxc_mipi_dsi mxc_mipi_dsi: buf[5]=0x0d05a713
mxc_mipi_dsi mxc_mipi_dsi: buf[6]=0x5517d410
mxc_mipi_dsi mxc_mipi_dsi: buf[7]=0x00030716
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x00000011
mxc_mipi_dsi mxc_mipi_dsi: buf[0]=0x00000029
backlight mipid-bl: mipid backlight bringtness:255.
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi_set_mode: cmd_mode 0x0.
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
mxc_mipi_dsi mxc_mipi_dsi: mipi_dsi IRQ status0:0x0, status1:0x80!
And I checked the reference manual, it says,
the 0x80 corresponds to bit7 dpi_pld_wr_err in 42.6.19 Interrupt status register 1 (MIPI_DSI_ERROR_ST1)
During a DPI pixel line storage the payload FIFO went full and data stored is corrupted.
Any ideas on this question?
Any guidance will be appreciated.
Thank you in advance.
Hello jamesbone,
I could set 200Mhz, 150MHz, even 100MHz to that max phy clock, but the same error comes out contineously.
So I guess there must be something strange out there that cause this problem.
Do you mean 150MHz will work well?
Hello Xueyuan,
I do not have a mipi display himax8369 or mipi-display with himax8363 to test, but we have test the max clock speed of the MIPI port display and it works with 150Mhz. And since you mention that with display himax8369 was working then it should be the frequency the problem.
Have a great day,
Jaime
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------