Could you explain me some points related to MIPI_CSI_PHY_STATE in imx6.
First of all 9-th bit. Active low. Is that mean that clk lane in ULPS if the bit equal zero value?
8-th bit. Clock lane actively receiving a DDR cloclk. Is that bit mean(1-value) that imx6 DPHY module clock is correctly configured. In my case it is always zero value.
Thanks.
解決済! 解決策の投稿を見る。
>Does it mean that imx6 mipi clock lane is in ULPS state if this bit equal zero?
yes
>Does it mean that it successfully receive clock from clk lane or from imx6 clock subsystem.
from clk lane
also from Debug steps for customer MIPI sensor.docx p.1
https://community.freescale.com/docs/DOC-94312
Tips:
In ov5640_mipi case (2 data lanes are used), the correct MIPI_CSI_PHY_STATE is
0x330 (and the bit 11 is jumping between 0 and 1, the value is jump between 0x330 and 0xb30).
Hi Fan
MIPI_CSI_PHY_STATE bit 9 : Active Low. This signal indicates that the Clock Lane
module has entered the Ultra Low Power state.
Suggest to look at MIPI_D-PHY_Specification for understanding clock behaviour
in ULPS state.
8-th bit. Clock lane actively receiving a DDR cloclk. Right, this means
that imx6 DPHY module clock is correctly configured.
For clock configuration one can check document
Debug steps for customer MIPI sensor.docx
https://community.freescale.com/docs/DOC-94312
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
igorpadykov wrote:
Suggest to look at MIPI_D-PHY_Specification for understanding clock behaviour
in ULPS state.
I know what mean ULPS mode towards MIPI dphy specification. I am interested in what this bit mean for imx6. Does it mean that imx6 mipi clock lane is in ULPS state if this bit equal zero?
igorpadykov wrote:
8-th bit. Clock lane actively receiving a DDR cloclk. Right, this means
that imx6 DPHY module clock is correctly configured.
For clock configuration one can check document
Debug steps for customer MIPI sensor.docx
I investigated this document. And configured CLK as it recommend. I also checked ¨mipi_pllref_clk¨ and ¨emi_clk¨ configuration. But I don`t understand still what mean 8-th bit.
What mean ¨actively receiving a DDR clock¨. Does it mean that it successfully receive clock from clk lane or from imx6 clock subsystem. Continuing the previous question, must 8-th bit be set in case of switched off ADV7280-m dphy and switched on imx6 dphy?
What correct value should be set in MIPI_CSI_PHY_STATE register before switching on ADV7280-m dphy?
Thanks.
>Does it mean that imx6 mipi clock lane is in ULPS state if this bit equal zero?
yes
>Does it mean that it successfully receive clock from clk lane or from imx6 clock subsystem.
from clk lane
also from Debug steps for customer MIPI sensor.docx p.1
https://community.freescale.com/docs/DOC-94312
Tips:
In ov5640_mipi case (2 data lanes are used), the correct MIPI_CSI_PHY_STATE is
0x330 (and the bit 11 is jumping between 0 and 1, the value is jump between 0x330 and 0xb30).