mfgtool, imx-usb-loader with SPL and u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfgtool, imx-usb-loader with SPL and u-boot

4,336件の閲覧回数
bba
Contributor III

Hello,

the default u-boot configuration for the imx6ul-evk use u-boot_2015.04. Here the compiled bootloader consist only of on singe u-boot binary u-boot.imx. These u-boot.imx file can be loaded via USB with the mfgtool as well as the imx-usb-loader imx_usb.

Using the fslc community version of the imx6ul-evk bsp the default bootloader is u-boot_2016.05. Here the compiled bootloader is divided into SPL and u-boot. I am able to load the SPL with the imx-usb-loader imx_usb or the mfgtool. But how can I load the following u-boot binary u-boot.img?

Is there any description available how to load the SPL followed by u-boot on the iMX6ul-EVK via USB boot?

Regards,

Birger

ラベル(3)
0 件の賞賛
4 返答(返信)

1,558件の閲覧回数
bba
Contributor III

Thanks for reply, we are using now the fsl u-boot version u-boot-imx_2015.04 instead of u-boot-fslc_2016.03. These version supports only u-boot.imx instead of SPL+u-boot.img.

Regards,

Birger

0 件の賞賛

1,558件の閲覧回数
mach
Contributor I

Hello Birger,

Sorry, I don't understand why uboot-2015.04  only supports u-boot.imx instead of SPL+u-boot.img. I noticed that the code of this uboot had been patched with the patches used to support SPL of imx6 sabresd.(https://community.nxp.com/message/864563 ) . Could you show me more details?

Best wishes,

Mc 

0 件の賞賛

1,558件の閲覧回数
bba
Contributor III

We only used the SPL+u-boot.img combination on iMX6ul-evk with eMMC. On the customer hardware we are using NAND. Here the OS and firmware will be transfered with the mfgtool booting via USB. As written by Igor above the recipes used to build a manufacturing tool image are

linux-imx-mfgtool and u-boot-mfgtool and supports only nxp uboot-imx without spl.

It can be possible that mfgtool image supports flashing SPL+u-boot.img, but we don't have any experience with that.

Regards,

Birger

0 件の賞賛

1,558件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Birger

the recipes used to build a manufacturing tool image are

linux-imx-mfgtool and u-boot-mfgtool and seems mfg tools support only

nxp uboot-imx without spl.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛