hi all,
I am using ov2710 parallel camera and pixel format used is IPU_PIX_FMT_GENERIC_16 .
I am able to capture an image,but it NOT coming in RGB format.
could please help me to find a way to convert generic 16 pixel format to rgb pixel format
解決済! 解決策の投稿を見る。
Hi,
You can convert it online using the website rawpixels.net.
I looked through the product info for OV2710 and saw that it supports only 8/10 bit raw data format. You will have to configure which stream the camera outputs by tweaking the camera registers. Assuming you are capturing 10-bit data, I think the format you should use for capturing is 0x30314742 (BG10) GitHub - avafinger/cap-v4l2: capture frames from CMOS camera ov5640 / ov8865 using V4l2 and OpenCV. The pixel format should be V4L2_PIX_FMT_SBGGR10.
hi igorpadykov;
Is there any external software tool to convert RAW image to RGB image format
Hi,
You can convert it online using the website rawpixels.net.
I looked through the product info for OV2710 and saw that it supports only 8/10 bit raw data format. You will have to configure which stream the camera outputs by tweaking the camera registers. Assuming you are capturing 10-bit data, I think the format you should use for capturing is 0x30314742 (BG10) GitHub - avafinger/cap-v4l2: capture frames from CMOS camera ov5640 / ov8865 using V4l2 and OpenCV. The pixel format should be V4L2_PIX_FMT_SBGGR10.
Hi Ayyappadas
unfortunately ipu does not support convertion generic/raw format to rgb as answered on
https://community.nxp.com/message/309833#309833
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------