matter err The user requested click

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

matter err The user requested click

195 次查看
tgt007
Contributor II

Hi NXP

The following error occurs when I compile imx93 matter imx-linux-nanbield-m imX-6.3-1.0.0. xml.

ERROR: Cannot install click because these package versions have conflicting dependencies.
|
| The conflict is caused by:
| The user requested click
| The user requested (constraint) click==8.1.3
|
| To fix this you could try to:
| 1. loosen the range of package versions you've specified
| 2. remove package versions to allow pip attempt to solve the dependency conflict
|
| ERROR: ResolutionImpossible: for help visit https://pip.pypa.io/en/latest/topics/dependency-resolution/#dealing-with-dependency-conflicts
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/ubuntu/imx-linux-nanbield/sources/meta-matter/recipes-matter/matter/matter.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 9974 tasks of which 9973 didn't need to be rerun and 1 failed.

 

How to solve?

thinks!

 

 

 

0 项奖励
回复
0 回复数