mapping RMII signals between iMX8XL ENET0 and TI's DP83TC811R PHY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mapping RMII signals between iMX8XL ENET0 and TI's DP83TC811R PHY

702件の閲覧回数
chirag_patel1
Contributor I

Hello

I'm trying to connect TI's DP83TC811R PHY in RMII mode to iMX8XL's ENET0 block. Can someone provide which pins to connect to on ENET0 ? Also what Alternate functions to use?

Thanks in advance.

0 件の賞賛
返信
1 返信

645件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chirags

rmii mapping example can be found in ENET 100 Mbps Daughter Card 

schematic:

i.MX8 MEK Base Board Design Files

i.MX8 RMII-BRPHY card Design Files

Alternate functions can be found in linux ..pinctrl/pads-imx8dxl.h

pads-imx8dxl.h\pinctrl\dt-bindings\include - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信