It always show me "Error: fail open file: >u-boot-imx8mm-evk-uuu.imx<-[?25h" when l try to executive the command of "uuu.exe uuu-android-mx8mm-evk-emmc.lst", How should l do?
Could you tell me your details steps? Which android version are you using? Are you using the prebuild images?
For the uuu downloading
• On Windows system, open the command line interface in administrator mode. The corresponding command is as
follows:
> .\uuu_imx_android_flash.bat -f imx8mm -a -e -u trusty
When the command above is executed, u-boot-imx8mm-trusty.imx with other default images will be flashed into eMMC
slot a for i.MX 8M Mini EVK.
I am using android_p9.0.0_1.0.0-ga_image_8mmevk downloaded from the official website
Win10 or Win7 pc are you using? I see your another question also meet the same problem.
Hi,
Does it work now? I see that you are using the i.MX 8M MiNi EVK, but when you download you were using the i.mx8mq images, it's for another board.
.\uuu_imx_android_flash.bat -f imx8mm -a -e
If it still not work contact me.
Have a nice day
Rita