Dear Team,
My customer is trying to build Yocto on imx8mm-lpddr4-evk.
These are the commands he used to download the repo and build the image:
python3 ./repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.2.xml
DISTRO=fsl-imx-xwayland MACHINE=imx8mm-lpddr4-evk source imx-setup-release.sh -b build_xwayland
bitbake imx-image-core
The complied is completed successfully but after flashing the image into the device there was no response from the device (did not bootup)?
Please advise if the procedure above is correct?
Waiting for your kind feedback, Thanks a lot.
KR,
Shai
what is your flashing commands ?
uuu -b emmc_all imx-boot-imx8qxpmek-sd.bin-flash imx-image-full-imx8qxpc0mek.wic.bz2
if flash is ok it shld hv some login to root message from ur debug port J11?
or u can run the demo test in the buld ?
1
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.2.xml
2 will support LPDDR4 / ddr4 board:
DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source imx-setup-release.sh -b build_xwayland
3
donot know yours uuu commands please shared here also ?
4
try to flash the demo image ok?
https://www.nxp.com/webapp/sps/download/preDownload.jsp
I've worked with the customer and we managed to flash the image into the iMX device.
since he builds the core image, it seems to be lack screen/display features.
if the customer would build the Multimedia does he need to do something in order to open the DSI port and display the xwayland feature or it's run by default?
Thanks in advance
KR,
Shai
Dear @joanxie and @josephzhou1,
Thanks for your input, it looks like there is an issue with my customer's image due to the DSI not working properly (he gets a Black screen).
he will try to rebuild the Yocto image and I will open a new thread as needed.
Thanks and regards,
Shai