integrating touchscreen in kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

integrating touchscreen in kernel

563 次查看
Ketki
Contributor I

I am using Goodix Touch driver with Android 9.0 and kernel 4+
I use pin 263 (GPIO4) as interrupt pin .
But I get the following error :

gpio-4 (GTP INT IRQ): _gpiod_direction_output_raw: tried to set a GPIO tied to an IRQ as output

I checked the pin is defined as input pin.So does this mean that some other driver is trying to use it as output pin. If yes how can I find this driver that is occupying the pin. I found an ads7428 driver in the device tree file occupying this pin and I disabled it . Other than that I can't find any other driver using the pin.

Thank You.

Regards,
Ketki K.

0 项奖励
回复
1 回复

556 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复