infinite error message of "[drm] No driver support for vblank timestamp query" during boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

infinite error message of "[drm] No driver support for vblank timestamp query" during boot

1,435 次查看
fei_4_xu
Contributor III

Hi,

 

I'm trying too bootup a new hardware board based on imx8qxp evk, I have flashed the official image of "L5.4.70-2.3.0_images" into the board and then switched to boot from mmc.

 

At the boot phase, the debug console prints infinite message like this:

[   24.714712] [drm] No driver support for vblank timestamp query.
[   24.720759] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[   24.729204] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[   24.736731] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[   24.758632] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

the message will never stop.

 

I'd like to check how to stop this message or how to locate the hardware errors if any.

 

Thanks.

0 项奖励
回复
1 回复

1,431 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Fei

 

official image of "L5.4.70-2.3.0_images" may not work on new hardware board as were

built for MEK board. For new custom board it is necessary to run ddr test and rebuild image

according to ddr test documentation

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/...

 

Best regards
igor

0 项奖励
回复