imx93x SDK 6.1.55 type-c ptn5150 Cannot be used normally,6.1.22 Running Properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx93x SDK 6.1.55 type-c ptn5150 Cannot be used normally,6.1.22 Running Properly

365 Views
gongyaxuan
Contributor I

Recently, I upgraded the SDK to 6.1.55 to adapt to the AB version cpu, but I found a problem after the upgrade, 6.1.22 is normal under the same defconfig, device tree and ptn5150 driver. 6.1.55 Driver Error Delayed Loading
I would like to know if 6.1.55 has modified those things, and how can I normally use ptn5150 type-c on 6.1.55

gongyaxuan_0-1708327184679.png

[ 2.254254] ptn5150 0-003d: failed to allocate register map: -517

Device tree with ptn5150 driver in attachment

0 Kudos
Reply
1 Reply

305 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @gongyaxuan

Thank you for contacting NXP Support.

There is no information that states the specific changes that could have problems with the driver and the libraries. However, you can start measuring the I2C signals that sends the i.MX93 with the BSP version 6.1.22 and 6.1.55.

 

0 Kudos
Reply