imx8qxpmek Yocto Build Faild

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qxpmek Yocto Build Faild

ソリューションへジャンプ
780件の閲覧回数
WolsYang
Contributor IV

Hi I am use imx8qxpmek, and I follow i.MX Yocto Project User's Guide, to do the step.

 

DISTRO=fsl-imx-wayland MACHINE=imx8qmmek source imx-setup-release.sh -b build

bitbake imx-image-full

echo "UBOOT_CONFIG = \"emmc\"" >> conf/local.conf

bitbake imx-image-full

At here I got an error

ERROR: imx-boot-1.0-r0 do_compile: Execution of 'build/tmp/work/imx8qxpmek-poky-linux/imx-boot/1.0-r0/temp/run.do_compile.3129740' failed with exit code 1
ERROR: Logfile of failure stored in:build/tmp/work/imx8qxpmek-poky-linux/imx-boot/1.0-r0/temp/log.do_compile.3129740

build/tmp/deploy/images/imx8qxpmek/u-boot-imx8qxpmek.bin-emmc': No such file or directory

So I follow IMX8M error building uboot for emmc with Yocto 

Add UBOOT_CONFIG[emmc] = "imx8qxp_mek_config,emmc" to  meta-imx/meta-bsp/conf/machine/imx8qxpmek.conf

then

bitbake imx-image-full

uuu emmc_all imx-boot imx8qxpmek-20211224032647.rootfs.wic.bz2

And  I got a fail

uuu (Universal Update Utility) for nxp imx chips -- lib1.4.182-5-g5397913

Success 0 Failure 1


3:9 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -scanterm -f ../../../imx-yocto-bsp/build/tmp/deploy/images/imx8qxpmek/imx-boot

I try to remove UBOOT_CONFIG[emmc] = "imx8qxp_mek_config,emmc" from  meta-imx/meta-bsp/conf/machine/imx8qxpmek.conf

but uuu got same error : (

Any one coluld help me? By the way I run on ubuntu20.

0 件の賞賛
返信
1 解決策
775件の閲覧回数
WolsYang
Contributor IV

For me, the fist problem, "do not" do "UBOOT_CONFIG = \"emmc\"" >> conf/local.conf

Because default BSP build can support both SD card and eMMC storage.

The second issue is my ENV error(imx8qmmek and imx8qxpmek)  : (

So  the final loader not fit my board.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
776件の閲覧回数
WolsYang
Contributor IV

For me, the fist problem, "do not" do "UBOOT_CONFIG = \"emmc\"" >> conf/local.conf

Because default BSP build can support both SD card and eMMC storage.

The second issue is my ENV error(imx8qmmek and imx8qxpmek)  : (

So  the final loader not fit my board.

0 件の賞賛
返信