imx8qxp copying camera video data is too slow!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp copying camera video data is too slow!

Jump to solution
1,111 Views
783435100
Contributor III

Dear technical support:
I use mx8_v4l2_cap_drm.c to test and collect image data, and add the code in the static int save_to_file(int ch, struct video_channel *video_ch)  function:
memcpy(cpu_buf,video_ch[ch].buffers[buf_id].planes[i].start,1280*720*2);
  It takes 20 milliseconds to execute this copy.
  Is there any way to shorten the copy time?  Such as DMA?
  Thank you!

0 Kudos
Reply
1 Solution
1,100 Views
igorpadykov
NXP Employee
NXP Employee

Hi 783435100

 

what processor revision used in the case, recommended to use latest rev.C0,

it improved image susystem performance as described in AN12770

i.MX 8X C0 Migration Guide Migrating from i.MX 8X B0 to i.MX 8X C0

Recommended to try copying on i.MX8QXP MEK board using latest linux release

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.47_2.2.0

 

Best regards
igor

View solution in original post

0 Kudos
Reply
4 Replies
1,101 Views
igorpadykov
NXP Employee
NXP Employee

Hi 783435100

 

what processor revision used in the case, recommended to use latest rev.C0,

it improved image susystem performance as described in AN12770

i.MX 8X C0 Migration Guide Migrating from i.MX 8X B0 to i.MX 8X C0

Recommended to try copying on i.MX8QXP MEK board using latest linux release

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.47_2.2.0

 

Best regards
igor

0 Kudos
Reply
1,081 Views
783435100
Contributor III

Is there a way?

0 Kudos
Reply
1,070 Views
igorpadykov
NXP Employee
NXP Employee

one can try copy with edma, M4 SDK has example in

..memory_to_memory /edma_memory_to_memory.c

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 Kudos
Reply
1,094 Views
783435100
Contributor III

I just use imx-yocto-L5.4.47_2.2.0

0 Kudos
Reply