imx8qxp ping ubuntu success, but ubuntu ping imx8qxp failed,what should i do ?
autolink_8q:/ # ping -I usb0 192.168.5.101
PING 192.168.5.101 (192.168.5.101) from 192.168.5.100 usb0: 56(84) bytes of data.
64 bytes from 192.168.5.101: icmp_seq=1 ttl=64 time=1.82 ms
64 bytes from 192.168.5.101: icmp_seq=2 ttl=64 time=2.43 ms
win@autolink-bsp:~$ ping -I enp0s20u12 192.168.5.100
PING 192.168.5.100 (192.168.5.100) from 192.168.5.101 enp0s20u12: 56(84) bytes of data.
(No response)
defconfig:
CONFIG_USB_USBNET=y
CONFIG_USB_NET_CDC_NCM=y
CONFIG_USB_F_NCM=y
CONFIG_USB_G_NCM=y
-------------------------------------------------------------------------------------------------------
imx8qxp:
autolink_8q:/ # ifconfig usb0 192.168.5.100 up
autolink_8q:/ # ifconfig
lo .... ...
usb0 Link encap:Ethernet HWaddr ce:54:f5:41:64:51
inet addr:192.168.5.100 Bcast:192.168.5.255 Mask:255.255.255.0
inet6 addr: fe80::cc54:f5ff:fe41:6451/64 Scope: Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:304 errors:0 dropped:0 overruns:0 frame:0
TX packets:65 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:42915 TX bytes:6836
wlan0 ... ...
---------------------------------------------------------------------------------------------------------
ubuntu :
win@autolink-bsp:~$ lsusb
Bus 003 Device 110: ID 0525:a4a1 Netchip Technology, Inc. Linux-USB Ethernet Gadget
win@autolink-bsp:~$ sudo ifconfig enp0s20u12 192.168.5.101 up
win@autolink-bsp:~$ ifconfig
enp0s20u12 Link encap:Ethernet HWaddr 2a:09:67:64:99:6d
inet addr:192.168.5.101 Bcast:192.168.5.255 Mask:255.255.255.0
inet6 addr: fe80::2809:67ff:fe64:996d/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:70 errors:0 dropped:0 overruns:0 frame:0
TX packets:305 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:3876 (3.8 KB) TX bytes:47241 (47.2 KB)
Hi win
some documents with ncm usage were sent you via mail.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------