Hi experts:
我依照 MX8X_4.14.98_ga_BootLoader_V5-20190903_chn.pdf i.mx8x启动代码定制文档
使用USBOTG1透過UUU下载 image (在i.MX8QXP MEK 上是连接到了底板的USBOTG 上),
打开其支持:
\uboot-imx\configs\imx8qxp_mek_defconfig
-# CONFIG_CI_UDC=y
+CONFIG_CI_UDC=y
同时, 把typeC 加USBOTG2/3 禁止掉:
-CONFIG_USB_TCPC=y
+#CONFIG_USB_TCPC=y
-CONFIG_USB_CDNS3=y
-CONFIG_USB_CDNS3_GADGET=y
+#CONFIG_USB_CDNS3=y
+#CONFIG_USB_CDNS3_GADGET=y
但因bootloader 包含了SPL 功能,
在imx-yocto-bsp\sources\meta-fsl-bsp-release\imx\meta-bsp\conf\machine\imx8qxpmek.conf會參考到imx8qxp_mek_spl_defconfig ,有如下的的定義:
UBOOT_CONFIG_SD = \
"${@bb.utils.contains('COMBINED_FEATURES', 'optee', 'imx8qxp_mek_spl_defconfig', \
'imx8qxp_mek_defconfig', d)}"
造成了透過UUU download 時terminal會停在如下訊息,
U-Boot SPL 2018.03-4.14.98-2.3.1+gb1840a04d7 (Jun 22 2020 - 02:08:53 +0000)
Normal Boot
Trying to boot from USB SDP
couldn't find an available UDC
g_dnl_register: failed!, error: -19
SDP: initialize...
但如果在machine\imx8qxpmek.conf 把'imx8qxp_mek_spl_defconfig刪除,則可正常下載,這樣的修改是否正確?
如果有secure boot及SPL 的須求,這樣的修改是否會影響功能?
麻煩提供uboot包含SPL 時,如何修改BSP才能使用USBOTG1 透過UUU正常下載 image?
謝謝
So, in the imx8qxp_mek_spl_defconfig, do you modify it same as you did on imx8qxp_mek_defconfig?
Yes, I also modify the imx8qxp_mek_defconfig as attached file
If we remove as below,
Add DISTRO_FEATURES_remove = " optee" in local.conf
And replace the defconfig using attachment can work.
Could you help to check the side effect after disable optee? And if we need secure boot , can it disable the optee ? if not , how to modify it?
Thank you.
Penny Lin