MX8X_4.14.98_ga_BootLoader_V5-20190903_chn.pdf i.mx8x启动代码定制文档

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8X_4.14.98_ga_BootLoader_V5-20190903_chn.pdf i.mx8x启动代码定制文档

No ratings
Comments

Thanks for sharing! 

Hi John,

Thanks for sharing. I want to bulid linux-imx in standalone environment, but the error appeared:

In file included from arch/arm64/boot/dts/al/alpine-v2-evp.dts:35:0:
arch/arm64/boot/dts/al/alpine-v2.dtsi:37:10: fatal error: dt-bindings/interrupt-controller/arm-gic.h: No such file or directory
#include <dt-bindings/interrupt-controller/arm-gic.h>
^~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
compilation terminated.
scripts/Makefile.lib:317: recipe for target 'arch/arm64/boot/dts/al/alpine-v2-evp.dtb' failed
make[2]: *** [arch/arm64/boot/dts/al/alpine-v2-evp.dtb] Error 1
scripts/Makefile.build:587: recipe for target 'arch/arm64/boot/dts/al' failed
make[1]: *** [arch/arm64/boot/dts/al] Error 2
arch/arm64/Makefile:138: recipe for target 'dtbs' failed
make: *** [dtbs] Error 2
make: *** Waiting for unfinished jobs....

Do you have the same error?

solved.

Dear Sir,

              The attachment is using for iMX8M mini, would you please help to offer the iMX8QX boot loader document? 

Many thanks for your helps

BR

William Huang

sorry and upload the right one

updated to v5 添加
usb/nandflash 定
制及其它

Version history
Last update:
‎01-16-2019 12:01 AM
Updated by: