HI NXP,
I use imx8qm android P OS on IMX8QM MEK BOARD. I found that flex can failed to initialize sometimes. the intialization failure probability is about five percent . please help to analysis the question. thanks a lot !
the log that flexcan failed to initialize is as follows:
[ 9.133580] CAN device driver interface
[ 9.138411] flexcan 5a8d0000.can: 5a8d0000.can supply xceiver not found, using dummy regulator
[ 9.147350] flexcan 5a8d0000.can (unnamed net_device) (uninitialized): Could not enable RX FIFO, unsupported core
[ 9.157624] flexcan 5a8d0000.can: registering netdev failed
[ 9.163904] flexcan 5a8e0000.can: 5a8e0000.can supply xceiver not found, using dummy regulator
[ 9.172731] flexcan 5a8e0000.can (unnamed net_device) (uninitialized): Could not enable RX FIFO, unsupported core
[ 9.183044] flexcan 5a8e0000.can: registering netdev failed
[ 9.189092] flexcan 5a8f0000.can: 5a8f0000.can supply xceiver not found, using dummy regulator
[ 9.197897] flexcan 5a8f0000.can (unnamed net_device) (uninitialized): Could not enable RX FIFO, unsupported core
[ 9.208193] flexcan 5a8f0000.can: registering netdev failed
Hi NXP,
I am facing similar issue that, my can01 and can2 is not enabling at all in IMX8qm i think it is enable in m4.
Please let us know how to enable on A-53, following logs after system boots
root@imx8qmmek:~# [ 35.927014] vref_1v8: disabling
[ 35.930173] epdev_on: disabling
[ 35.933383] SD1_SPWR: disabling
[ 35.936594] can01-en: disabling
[ 35.939788] can2-en: disabling
[ 35.942853] can01-stby: disabling
[ 35.946209] can2-stby: disabling
[ 64.599200] cfg80211: failed to load regulatory.db
Please let me know changes has to be
using imx8qm-mek.dtb
i.MX Linux Yocto Project BSP 5.4.47_2.2.0 Release
Thanks and Regards,
rahulM
Hi yingjin
one can check on below link Android documentation (Release Notes, p1)
if approriate release used in the case, as not all releases support i.MX8QM.
For example P9.0.0_2.3.5 supports only i.MX8QXP.
i.MX Software and Development Tools | NXP
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi igorpadykov,
I found flexcan init fail sometimes , the failure probability is five percent. the success probalibity is ninety five percent.
So please analysis the question. because the imx8qm mek board has the same question when reboot system.