imx8qm converts the MIPI DSI into HDMI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8qm converts the MIPI DSI into HDMI

617 次查看
linjermmy
Contributor I

Dear experts,

 

I used imx8qm and adv7535 to convert the MIPI DSI into HDMI and outputted to monitor.

I have to output the video with resolution of 1920*720.

After set the dedicated edid (1920*720) table, there was no output on the monitor (monitor supports 1920*720) but it could show with resolution of 1920*1080.

Could you help me check whether there are any limitations for MIPI DSI to output video with resolution of 1920*720?  

0 项奖励
回复
1 回复

514 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Lin,

I’m afraid that i.MX8QM family is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 项奖励
回复