imx8mq DDR stress Tool Can't Calibration on 3GB(LPDDR4)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mq DDR stress Tool Can't Calibration on 3GB(LPDDR4)

767件の閲覧回数
raisaacwu
Contributor I

Hi,

I have Micron LPDDR4 SDRAM Type is MT53E768M32D2(attach spec file 200b_z2bm_ddp_s_lpddr4_53E.pdf).
MSCALE_DDR_Tool seems doesn't support this type dram. I use MX8M_LPDDR4_RPA_v22.xlsx to generate .ds file
that never reference ADDRMAP_ROW_B16(ADDRMAP7). In my understanding this dram type need use more than MX8M_LPDDR4_RPA_v22.xlsx's
default row bits. If not ,MX8M_LPDDR4_RPA_v22.xlsx how to fit in this dram type. If yes, Did any new update RPA.xlsx
for this dram. Thanks.

0 件の賞賛
2 返答(返信)

562件の閲覧回数
raisaacwu
Contributor I

Hi,

   This is my using 24 RPA.xlsx logout info(Z2BN_12G_2_1_24_17_10_3_32.log). And success embedded those gen code (ddr_init & ddrphy_train)in my system. But there is some problem for access memory space. There can't reach over 2GB space in this solution. In my logout info there shows "Total density detected on the board is: 1536MB ",, Does that correct? Any way I stand corrected..Thankful.

0 件の賞賛

562件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raisaac

there is v.24 RPA.xlsx on ddr test link

i.MX8 MSCALE SERIES DDR Tool Release (V3.00) 

Seems there is no problem to set necessary row address

pastedImage_2.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛