imx8mp mipi_dsi clock stops when provided to eDP bridge sn65dsi86

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp mipi_dsi clock stops when provided to eDP bridge sn65dsi86

1,063件の閲覧回数
shlomz
Contributor I

Hi,

I have a custom board (and a solidrun EVB with the same behavior) which has TI's eDP bridge sn65dsi86.

when using a refclk the bridge/display works fine but when providing it with the mipi_dsi clocks (after disconnecting the ext clk) it fails with edp errors:

[ 6.570668] ti_sn65dsi86 1-002c: [drm:ti_sn_bridge_enable [ti_sn65dsi86]] *ERROR* Can't read lane count (-110); assuming 4
[ 7.092286] ti_sn65dsi86 1-002c: [drm:ti_sn_bridge_enable [ti_sn65dsi86]] *ERROR* Can't read eDP rev (-110), assuming 1.1
[ 7.432894] ti_sn65dsi86 1-002c: [drm:ti_sn_bridge_enable [ti_sn65dsi86]] *ERROR* Can't read max rate (-110); assuming 5.4 GHz
[ 7.765867] ti_sn65dsi86 1-002c: [drm:ti_sn_bridge_enable [ti_sn65dsi86]] *ERROR* Link training failed, link is off (-5)

when the bridge module loads i can see the dsi clock goes up and down once and then stops.

I'm working on kernel 5.15 (also tried 5.10 on solidruns EVB). these are the dts nodes:

sn65dsi86: sn65dsi86@2d {

...

          clocks = <&mipi_dsi 0>,
          <&clk IMX8MP_VIDEO_PLL1_OUT>;

         clock-names = "mipi_clk", "video_pll";

...

}

mipi_dsi: mipi_dsi@32e60000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx8mp-mipi-dsim";
#clock-cells = <1>;
reg = <0x32e60000 0x10000>;
clocks = <&media_blk_ctrl IMX8MP_CLK_MEDIA_BLK_CTRL_MIPI_DSI_PCLK>,
<&media_blk_ctrl IMX8MP_CLK_MEDIA_BLK_CTRL_MIPI_DSI_CLKREF>;
clock-names = "cfg", "pll-ref";
assigned-clocks = <&clk IMX8MP_CLK_MEDIA_MIPI_PHY1_REF>;
assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
assigned-clock-rates = <12000000>;
interrupts = <GIC_SPI 18 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&mipi_phy1_pd>;
status = "disabled";

port@0 {
dsim_from_lcdif: endpoint {
remote-endpoint = <&lcdif_to_dsim>;
};
};
};

I tried various clocks (like IMX8MP_VIDEO_PLL1_OUT) and also to re-parent the dsi from IMX8MP_CLK_24M (which fails on dtc compilation).

would appreciate any help,

thanks!

0 件の賞賛
返信
8 返答(返信)

1,040件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,032件の閲覧回数
shlomz
Contributor I

Hi  joanxie,

I've already gone over their patch and did not find anything related to the mipi_dsi clock

any other suggestions?

thanks.

0 件の賞賛
返信

992件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

sn65dsi86  doesn't supported by the default bsp, so I couldn't share any sample with you, could you share the full dts files here? let me double check it

0 件の賞賛
返信

950件の閲覧回数
shlomz
Contributor I

Hi,

regardless of my specific bridge, how do u define the mipi_dsi phy clock to be used externally with an attached bridge? (kernel 5.15)

0 件の賞賛
返信

944件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mean this clock?

joanxie_0-1703232413087.png

this depends on your own display, the formula is Fout=Fin*(M / (P * 2 ^ S)), current bsp use12Mhz for Fin

0 件の賞賛
返信

863件の閲覧回数
shlomz
Contributor I

HI,

can you please elaborate on the formula, its parameters and how should the output value be used?

I've used the same clock in my bridge' node:

clocks = <&clk IMX8MP_CLK_MEDIA_MIPI_PHY1_REF>;
clock-names = "pll-ref";
assigned-clocks = <&clk IMX8MP_CLK_MEDIA_MIPI_PHY1_REF>;
assigned-clock-parents = <&clk IMX8MP_CLK_24M>;
assigned-clock-rates = <12000000>;

 

 

0 件の賞賛
返信

607件の閲覧回数
jocker-xie
Contributor I

Have you solved this problem? I am also encountering this problem with IMX8MM.

0 件の賞賛
返信

833件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

when using a refclk the bridge/display works fine but when providing it with the mipi_dsi clocks (after disconnecting the ext clk) it fails with edp error

>why do you change the refclk to the mipi dsi clocks? pls provide you full dts file to check

0 件の賞賛
返信