I am developing a 2-channel camera with DART-MX8M-PLUS.
CAM -> PR2000K(HD Receiver with MIPI output) -> imx8mp
PR2000K only supports clock continuous mode. No non-continuous mode.
csi2-0 works normally, but csi2-1 cannot get a start frame. Strangely, sometimes it works.
Below are the dts file settings.
pr2000k_mipi1: pr2000k_mipi@5c { port { pr2000k_mipi0: pr2000k_mipi@5f { port { |
&mipi_csi_0 { port@0 { &mipi_csi_1 { port@1 { |
Debug message of imx8-mipi-csi2-sam.c
csi2-1 cannot get a start frame like below.
[ 167.160218] mxc-mipi-csi2.0: mipi_csis_s_stream: 1, state: 0x0 [ 167.160329] mxc-mipi-csi2.0: mipi_csis_imx8mp_phy_reset: bus fmt is 12 bit ! [ 167.160368] mxc-mipi-csi2.0: fmt: 0x2006, 1280 x 960 [ 167.160405] mxc-mipi-csi2.0: Frame Start: 1 [ 167.160410] mxc-mipi-csi2.0: status: 01000000 [ 167.176222] mxc-mipi-csi2.0: --- mipi_csis_s_stream --- [ 167.176234] mxc-mipi-csi2.0: CSIS_VERSION[0]: 0x03060301 [ 167.176241] mxc-mipi-csi2.0: CSIS_CMN_CTRL[4]: 0x00004b05 [ 167.176247] mxc-mipi-csi2.0: CSIS_CLK_CTRL[8]: 0x000f0000 [ 167.176252] mxc-mipi-csi2.0: CSIS_INTMSK[10]: 0x0fffff1f [ 167.176258] mxc-mipi-csi2.0: CSIS_INTSRC[14]: 0x00000000 [ 167.176264] mxc-mipi-csi2.0: CSIS_DPHYSTATUS[20]: 0x00000000 [ 167.176270] mxc-mipi-csi2.0: CSIS_DPHYCTRL[24]: 0x0300001f [ 167.176276] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_L[30]: 0x000001f4 [ 167.176283] mxc-mipi-csi2.0: CSIS_DPHYBCTRL_H[34]: 0x00000000 [ 167.176289] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_L[38]: 0x00000000 [ 167.176295] mxc-mipi-csi2.0: CSIS_DPHYSCTRL_H[3c]: 0x00000000 [ 167.176301] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH0[40]: 0x00001078 [ 167.176306] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH1[50]: 0x000008fd [ 167.176313] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH2[60]: 0x000008fe [ 167.176319] mxc-mipi-csi2.0: CSIS_ISPCONFIG_CH3[70]: 0x000008ff [ 167.176325] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH0[44]: 0x03c00500 [ 167.176330] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH1[54]: 0x80008000 [ 167.176336] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH2[64]: 0x80008000 [ 167.176342] mxc-mipi-csi2.0: CSIS_ISPRESOL_CH3[74]: 0x80008000 [ 167.176348] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH0[48]: 0x00000000 [ 167.176354] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH1[58]: 0x00000000 [ 167.176359] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH2[68]: 0x00000000 [ 167.176365] mxc-mipi-csi2.0: CSIS_ISPSYNC_CH3[78]: 0x00000000 [ 167.176371] mxc-mipi-csi2.0: --- mipi_csis_s_stream --- [ 167.176376] mxc-mipi-csi2.0: GPR_GASKET_0_CTRL[60]: 0xffff8000 [ 167.176384] mxc-mipi-csi2.0: GPR_GASKET_0_HSIZE[64]: 0xffff8000 [ 167.176389] mxc-mipi-csi2.0: GPR_GASKET_0_VSIZE[68]: 0xffff8000 [ 167.192412] mxc-mipi-csi2.0: Frame End: 1 [ 167.192426] mxc-mipi-csi2.0: status: 00100000 [ 167.193739] mxc-mipi-csi2.0: Frame Start: 2 [ 167.193752] mxc-mipi-csi2.0: status: 01000000 [ 167.225753] mxc-mipi-csi2.0: Frame End: 2 [ 167.225768] mxc-mipi-csi2.0: status: 00100000 [ 167.227075] mxc-mipi-csi2.0: Frame Start: 3 [ 167.227090] mxc-mipi-csi2.0: status: 01000000 |
[ 202.392216] mxc-mipi-csi2.1: mipi_csis_s_stream: 1, state: 0x0 [ 202.392333] mxc-mipi-csi2.1: mipi_csis_imx8mp_phy_reset: bus fmt is 12 bit ! [ 202.392372] mxc-mipi-csi2.1: fmt: 0x2006, 1280 x 960 [ 202.408216] mxc-mipi-csi2.1: --- mipi_csis_s_stream --- [ 202.408228] mxc-mipi-csi2.1: CSIS_VERSION[0]: 0x03060301 [ 202.408235] mxc-mipi-csi2.1: CSIS_CMN_CTRL[4]: 0x00004b05 [ 202.408241] mxc-mipi-csi2.1: CSIS_CLK_CTRL[8]: 0x000f0000 [ 202.408246] mxc-mipi-csi2.1: CSIS_INTMSK[10]: 0x0fffff1f [ 202.408252] mxc-mipi-csi2.1: CSIS_INTSRC[14]: 0x00000000 [ 202.408258] mxc-mipi-csi2.1: CSIS_DPHYSTATUS[20]: 0x000000f2 [ 202.408266] mxc-mipi-csi2.1: CSIS_DPHYCTRL[24]: 0x0300001f [ 202.408271] mxc-mipi-csi2.1: CSIS_DPHYBCTRL_L[30]: 0x000001f4 [ 202.408279] mxc-mipi-csi2.1: CSIS_DPHYBCTRL_H[34]: 0x00000000 [ 202.408285] mxc-mipi-csi2.1: CSIS_DPHYSCTRL_L[38]: 0x00000000 [ 202.408291] mxc-mipi-csi2.1: CSIS_DPHYSCTRL_H[3c]: 0x00000000 [ 202.408296] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH0[40]: 0x00001078 [ 202.408302] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH1[50]: 0x000008fd [ 202.408308] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH2[60]: 0x000008fe [ 202.408314] mxc-mipi-csi2.1: CSIS_ISPCONFIG_CH3[70]: 0x000008ff [ 202.408322] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH0[44]: 0x03c00500 [ 202.408327] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH1[54]: 0x80008000 [ 202.408335] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH2[64]: 0x80008000 [ 202.408341] mxc-mipi-csi2.1: CSIS_ISPRESOL_CH3[74]: 0x80008000 [ 202.408347] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH0[48]: 0x00000000 [ 202.408353] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH1[58]: 0x00000000 [ 202.408358] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH2[68]: 0x00000000 [ 202.408365] mxc-mipi-csi2.1: CSIS_ISPSYNC_CH3[78]: 0x00000000 [ 202.408371] mxc-mipi-csi2.1: --- mipi_csis_s_stream --- [ 202.408376] mxc-mipi-csi2.1: GPR_GASKET_0_CTRL[60]: 0xffff8000 [ 202.408382] mxc-mipi-csi2.1: GPR_GASKET_0_HSIZE[64]: 0xffff8000 [ 202.408388] mxc-mipi-csi2.1: GPR_GASKET_0_VSIZE[68]: 0xffff8000 |
This is similar to the post above.
Are both 2 channels not captured in continuous mode?
Should I redesign with a different receiver chip?
Thanks in advance.
Best regards,
Jayden
已解决! 转到解答。
Hi @Jayden_Soon,
Hi @Jayden_Soon,