imx8mm qt opengl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm qt opengl

1,465 Views
lizuobin
Contributor II

Hello,

      I found some problems when testing imx8mm evk.

      /usr/share/qt5/examples/opengl/qopenglwidget/qopenglwidget

QQ图片20190508121908.jpg

 Text and partial graphics are drawn incorrectly, you can see the background of the weston,

How to solve this problem?

0 Kudos
Reply
3 Replies

1,309 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello li,

There must be some missconfiguration in color of the LCD, to be frankly try to burn the image again if the same issue happens then try to change the configuration of the LCD.

Regards

0 Kudos
Reply

1,309 Views
lizuobin
Contributor II

HI,

thanks for your reply,I am using the image provided in L4.14.98_2.0.0_ga_images_MX8MMEVK, I don't think this is a problem with the LCD driver, because only opengl related programs will have the above problem.

thanks.

0 Kudos
Reply

1,005 Views
sakizci
Contributor II

Hello li,

did you solve this problem? if you solved it can you share it with me ?

Thanks

0 Kudos
Reply