imx8mm evk gpt driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm evk gpt driver

1,916 Views
andyli
Contributor II

hi 

   my using board is imx8mm evk, need to use GPT to create interrupt every 1ms to do my IRS,

   I have some questions.

  1, it has 6 GPT, whether it is all the same, customer can use any one

   2.kernel 4.9.124, it can not support imx8 GPT in the file of timer-imx-gpt.c. at last I found that it is  using imx7d_timer, 

it is compatible with "mx7d_timer, "fsl,imx7d-gpt"

    gpt1: gpt@302d0000 {
        compatible = "fsl,imx8mq-gpt", "fsl,imx7d-gpt";

 in timer_imx_gpt.c CLOCKSOURCE_OF_DECLEAR(mx7d_time,fsl,imx7d-gpt,imx6dl_timer_init_dt)

my question is imx8 timer using imx6 driver in the timer-imx-gpt.c.

3. I grep the fsl-imx8mm.dtsi, fsl-imx8mm_evk.dts, it can not config the gpt, how to config gpt in dts

4. could you give me some example about gpt,  how to test it can work well.

 

 

0 Kudos
Reply
5 Replies

1,793 Views
edcloudcycle
Contributor III

Hi @igorpadykov 

I would also like to use the gpt under Linux. Is there a way to do it? It seems like a driver is present in the kernel. 

Thanks
Ed

0 Kudos
Reply

1,912 Views
igorpadykov
NXP Employee
NXP Employee

Hi andyli

 

>1, it has 6 GPT, whether it is all the same, customer can use any one


all the same

 

> 2..my question is imx8 timer using imx6 driver in the timer-imx-gpt.c.

yes


>3. I grep the fsl-imx8mm.dtsi, fsl-imx8mm_evk.dts, it can not config the gpt, how to config gpt in dts
>4. could you give me some example about gpt, how to test it can work well.

 

gpt is used by M4 core, please refer to SDK_EVK-MIMX8MM folder ../driver/examples/gpt

https://mcuxpresso.nxp.com/en/welcome

also may be useful:

https://community.nxp.com/t5/i-MX-Processors/GPT-capture-sample-on-M4-seems-to-hang-on-Linux-boot/m-...

 

Best regards
igor

 

0 Kudos
Reply

1,876 Views
andyli
Contributor II

hello igor
        It has the configuration of GPT in kernel 4.x version in file Fsl-imx8mq.dtsi, but it has been removed in Kernel5.4. I wonder why.
Can you give me an idea of how GPT should be used in i.mx8mm evk.

0 Kudos
Reply

1,884 Views
aaron_zeng
Contributor II

hello igor

I saw the comments at “timer-imx-gpt.c”  which in L5.4.24-2.1.0:

/*
 * There are 4 versions of the timer hardware on Freescale MXC hardware.
 *  - MX1/MXL
 *  - MX21, MX27.
 *  - MX25, MX31, MX35, MX37, MX51, MX6Q(rev1.0)
 *  - MX6DL, MX6SX, MX6Q(rev1.1+)
 */

Any patch for imx8m ?

0 Kudos
Reply

1,908 Views
andyli
Contributor II

HI 

   thanks for reply so fast

   "gpt is used by M4 core" means that no gpt modules in A53 core. 

    is it right or wrong?