imx8mm Android version ECM with AG35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mm Android version ECM with AG35

1,040 Views
fanxiaoyun
Contributor I

imx8mm Android9 communicate with AG35 through USB, imx8mm is HOST, and AG35 (4g module ,Quectel)is slave,but there must be  something wrong with android config, cause same kernel source code in linux version works ok, but android fails.

Cdc_ether and usbnet are builtin module. Kenel log shows that usb is recognized, I manually ifconfig usb0 up and set a ip to it, but still cannot ping through it.  Error shows "unreachable network". 

kernel log :

[ 84.045145] cdc_ether 1-1.3:1.4 usb0: unregister 'cdc_ether' usb-ci_hdrc.1-1.3, CDC Ethernet Device
[ 85.801652] usb 1-1.3: new high-speed USB device number 5 using ci_hdrc
[ 85.933836] usb 1-1.3: New USB device found, idVendor=2c7c, idProduct=0435
[ 85.940731] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 85.948212] usb 1-1.3: Product: LTE Module
[ 85.952331] usb 1-1.3: Manufacturer: Quectel, Incorporated
[ 85.957934] usb 1-1.3: SerialNumber: ecde80c
[ 85.984406] cdc_ether 1-1.3:1.4 usb0: register 'cdc_ether' at usb-ci_hdrc.1-1.3, CDC Ethernet Device, 22:f1:41:57:a1:30

Labels (1)
0 Kudos
Reply
2 Replies

1,014 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Have you tried contacting quectel?

I see that they have an Android Driver user guide in their webpage:

https://www.quectel.com/product/lte-ag35-automotive-module

Best regards,
Aldo.

0 Kudos
Reply

1,007 Views
fanxiaoyun
Contributor I

Hi,

I had contacted quectel at the first time,and patch code is most about the option.c, the driver about ecm is not involved.

The "usb0" network device is already recognized,and could be assigned a ip manually.

ifconfig usb0 up

ifconfig usb0 192.168.225.3

ping 192.168.225.1  failed.  //192.168.225.1 is the ip of  AG35.

0 Kudos
Reply