imx8 pinctrl generated by Pins tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 pinctrl generated by Pins tool

1,209 Views
xiaokaoy
Contributor I

Hello

I have a pin_mux.dts file generated by Pins tool which contains these two lines:
SC_P_QSPI0A_SCLK_LSIO_GPIO3_IO16 0x20000040
SC_P_QSPI0A_SS0_B_LSIO_GPIO3_IO14 0x00000020

The two macros are defined in pads-imx8qxp.h like this:
#define SC_P_QSPI0A_SCLK_LSIO_GPIO3_IO16 SC_P_QSPI0A_SCLK 4
#define SC_P_QSPI0A_SS0_B_LSIO_GPIO3_IO14 SC_P_QSPI0A_SS0_B 4
where 4 means ALT4, I think.

According to Page 1026 of i.MX 8DualX/8DualXPlus/8QuadXPlus Applications Processor Reference Manual,
bits 29-27 of the pad/mux control register for QSPI0A_SS0_B mean:
mux_mode
000b - LSIO_QSPI0A_SS0_B
100b - LSIO_GPIO3_IO14

In that case, why is 0x00000020, rather than 0x20000020, generated by Pins tool for SC_P_QSPI0A_SS0_B_LSIO_GPIO3_IO14.
Is it because the definition of SC_P_QSPI0A_SS0_B_LSIO_GPIO3_IO14 has already contained the number 4?
If that's the case, why is 0x20000040, rather than 0x00000040, is generated for SC_P_QSPI0A_SCLK_LSIO_GPIO3_IO16?

Another question is:
According to the Reference Manual, bits 31 and 30 of the mux/pad control register mean
bit 31
update lock for mux control
write 1 to allow programming to mux control [29:19]
bit 30
update lock for pad control
write 1 to allow programming to pad control [14-1:0]

What does 'write 1 to allow programming' mean here?
For example, in the case of above-mentioned 0x00000020, the bits 29:19 and 14-1:0 are actually useless/ignored, aren't they?

0 Kudos
Reply
2 Replies

1,176 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi Xiaokaoy,

 

Could you please specify the version of your board?, like which revision is the one that you have and, if it is an IMX8MM/IMX8QM-EVK etc.

This in order to know which file generate the pins tool.

 

Regards,

Israel H.

0 Kudos
Reply

1,132 Views
xiaokaoy
Contributor I

Thanks for your reply, Israel. The board was designed by hardware engineers of my company, which uses 

the i.MX8 DualX processor.
0 Kudos
Reply