imx8 Quad Max MEK The USB-C port does not work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8 Quad Max MEK The USB-C port does not work

1,085件の閲覧回数
cesar_miguel
Contributor II

Hello friends.
I have a problem with the imx8 Quad Max MEK. I can't use the USB-C port. The problem is than Windows 10 and Ubuntu 18.04 don't find it. It does not even exist as an unknown device. I trying use UUU for Android demo image. 

Any idea what the problem is?

ラベル(1)
タグ(2)
0 件の賞賛
4 返答(返信)

881件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Could you try using a different cable and also a different USB port on your host side?

seems like the USB isn't being powered correctly.

 

Best regards,
Aldo.

0 件の賞賛

881件の閲覧回数
cesar_miguel
Contributor II

Hello.

I have tried with different cables and USB ports. I think the port of the card does not work

0 件の賞賛

881件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hi,

 

Thanks for the update,

could you help me with these questions please.

You see any damage to the power supply cable?

Or to the Power input DIN connector (j9)?

Were you able to boot with the pre-built NXP Linux binary demo image of your kit?

 

Thank you,

Best regards,

Aldo.

0 件の賞賛

881件の閲覧回数
cesar_miguel
Contributor II

Hi,
- The cable of power supply is doesn't any damage.
-Any cable is damage
-The conector is perfect
- I did can't boot the pre-built NXP Linux binary demo image

thanks 

César

0 件の賞賛