imx8 Quad Max MEK The USB-C port does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8 Quad Max MEK The USB-C port does not work

1,044 Views
cesar_miguel
Contributor II

Hello friends.
I have a problem with the imx8 Quad Max MEK. I can't use the USB-C port. The problem is than Windows 10 and Ubuntu 18.04 don't find it. It does not even exist as an unknown device. I trying use UUU for Android demo image. 

Any idea what the problem is?

Tags (2)
0 Kudos
4 Replies

840 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Could you try using a different cable and also a different USB port on your host side?

seems like the USB isn't being powered correctly.

 

Best regards,
Aldo.

0 Kudos

840 Views
cesar_miguel
Contributor II

Hello.

I have tried with different cables and USB ports. I think the port of the card does not work

0 Kudos

840 Views
AldoG
NXP TechSupport
NXP TechSupport

Hi,

 

Thanks for the update,

could you help me with these questions please.

You see any damage to the power supply cable?

Or to the Power input DIN connector (j9)?

Were you able to boot with the pre-built NXP Linux binary demo image of your kit?

 

Thank you,

Best regards,

Aldo.

0 Kudos

840 Views
cesar_miguel
Contributor II

Hi,
- The cable of power supply is doesn't any damage.
-Any cable is damage
-The conector is perfect
- I did can't boot the pre-built NXP Linux binary demo image

thanks 

César

0 Kudos