Hi,
I'm porting a BCM4343W WIFI driver from an imx7dsabresd to a imx7 Warp7 board and I need to prevent to WIFI driver from loading on boot as its causing a kernel panic. I'd like to get the OS running then run the driver manually.
What is the recommended way to disable this? Can I disable it simply in the boot process or does it require an out-of-tree module which I modprobe at another time?
BR,
Ed
Hi Edward
one can look at BCM4339 driver which could be modprobed,
it is described in attached Linux Manual Chapter 46 Wi-Fi BCM4339 Driver.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks, but how can I disable it in the first place from running on boot?
BR,
Ed