Hi NXP FAE,
I got a imx7d sabresd board (RevD) and EBookDC4, boot disk is SDCard, provided by NXP,
the image version is linux-4.1.15_1.2.0A.
I boot the device, found
cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)
imx_epdc_v2_fb 306f0000.epdc: Direct firmware load for imx/epdc/epdc_ED060XH2C1.fw failed with error -2
imx_epdc_v2_fb 306f0000.epdc: Falling back to user helper
but the firmware epdc_ED060XH2C1.fw could be found in /lib/firmware/imx/epdc, why did fimware load fail?
Regards,
David
Original Attachment has been moved to: imx7.log.zip
已解决! 转到解答。
Dear Igor,
Thanks for your reply, my EbookDC4 can work well, I only wonder why direct firmware load fails,
maybe the kernel file system isn't ready? I guess.
static int fw_get_filesystem_firmware(struct device *device,
struct firmware_buf *buf)
{
......
snprintf(path, PATH_MAX, "%s/%s", fw_path[i], buf->fw_id);
printk("__FUNCTION__, path: %s\n", path);
file = filp_open(path, O_RDONLY, 0);
printk("__FUNCTION__, error: %x\n", IS_ERR(file));
.....
}
log is as follows:
__FUNCTION__, path: /lib/firmware/updates/4.1.15+g77f6154/imx/epdc/epdc_ED060XH2
C1.fw
__FUNCTION__, error: 1
__FUNCTION__, path: /lib/firmware/updates/imx/epdc/epdc_ED060XH2C1.fw
__FUNCTION__, error: 1
__FUNCTION__, path: /lib/firmware/4.1.15+g77f6154/imx/epdc/epdc_ED060XH2C1.fw
__FUNCTION__, error: 1
__FUNCTION__, path: /lib/firmware/imx/epdc/epdc_ED060XH2C1.fw
__FUNCTION__, error: 1
Hi David
please check that correct dtb file is selected (imx7d-sdb-epdc.dtb) as
answered by Mark Ruthenbeck at 27.07.2016 10:12
connecting i.MX7D Sabre(MCIMX7SABRE) and E-INK panel(IMXEBOOKDC4)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor,
I have modified uboot env setting,
a.) setenv fdt_file imx7d-sdb-epdc.dtb
(originally this is "fdt_file=imx7d-sdb.dtb")
b.) setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=${mmcroot} epdc video=mxcepdcfb:ED060XH2C1,bpp=16'
run unitestunit_tests# ./mxc_epdc_v2_fb_test.out
EBookDC4 runs ok, but the issue still exists.
imx_epdc_v2_fb 306f0000.epdc: Direct firmware load for imx/epdc/epdc_ED060XH2C1.
fw failed with error -2
imx_epdc_v2_fb 306f0000.epdc: Falling back to user helper
Regards,
David
Hi David
please try Demo Images
There is NO need to add the "epdc video= args as suggested on
connecting i.MX7D Sabre(MCIMX7SABRE) and E-INK panel(IMXEBOOKDC4)
Best regards
igor
Dear Igor,
Thanks for your reply, my EbookDC4 can work well, I only wonder why direct firmware load fails,
maybe the kernel file system isn't ready? I guess.
static int fw_get_filesystem_firmware(struct device *device,
struct firmware_buf *buf)
{
......
snprintf(path, PATH_MAX, "%s/%s", fw_path[i], buf->fw_id);
printk("__FUNCTION__, path: %s\n", path);
file = filp_open(path, O_RDONLY, 0);
printk("__FUNCTION__, error: %x\n", IS_ERR(file));
.....
}
log is as follows:
__FUNCTION__, path: /lib/firmware/updates/4.1.15+g77f6154/imx/epdc/epdc_ED060XH2
C1.fw
__FUNCTION__, error: 1
__FUNCTION__, path: /lib/firmware/updates/imx/epdc/epdc_ED060XH2C1.fw
__FUNCTION__, error: 1
__FUNCTION__, path: /lib/firmware/4.1.15+g77f6154/imx/epdc/epdc_ED060XH2C1.fw
__FUNCTION__, error: 1
__FUNCTION__, path: /lib/firmware/imx/epdc/epdc_ED060XH2C1.fw
__FUNCTION__, error: 1