Hi
你试一下L5.4.70_2.3.0,我们的新BSP都是兼容6ULL的
BR
Zhiming
Hi,
因为我使用的板子除了emmc的位宽不一样,其他都一样,官方的下载工具也能直接使用,但是就是编译出来的yocto不能使用。还有就是我换过5.4.24-2.1.0这个版本也是不行。
Hi
你把错误信息贴上来
是5.4.24-2.1.0这个版本的错误信息吗
对
首先L4和L5的版本差异很大,其次L5也是支持i.mx6ull的,编译出来的系统和demo系统可能会有一点差异,不过不会影响系统启动。你之前说emmc位宽不一样,你是修改改的内核还是uboot,如果位宽不一样,uboot和kernel的驱动代码都需要修改。
Hi
目前我无法给出准确的原因,你看一下这个教程:https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/README.log?h=imx_v2020.04_5.4.70_2.3.0
打开uboot的debug模式,看一下在下载的时候卡在了哪里
U-Boot 2016.03-imx_v2016.03_4.1.15_2.0.0_ga+ga57b13b (Mar 23 2021 - 19:10:33 +0800)
CPU: Freescale i.MX6ULL rev1.1 69 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 50C
Reset cause: POR
Board: MX6ULL 14x14 EVK
I2C: ready
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment
Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
Net: Board Net Initialization Failed
No ethernet found.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic!
=>
=>
=> <INTERRUPT>
=>
=>
=>
4.1.15_2.0.0当我处在下载端是,还是可以进行输入的
当我使用4.1.15-2.10这个版本是uboot还是能使用的,而这个版本uboot都无法使用。
信息如下:
U-Boot 2020.04-5.4.24-2.1.0+g4979a99482 (Mar 25 2021 - 08:52:02 +0000)
CPU: i.MX6ULL rev1.1 792 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 46C
Reset cause: POR
Model: i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
[*]-Video Link 0 (480 x 272)
[0] lcdif@21c8000, video
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
Net: Could not get PHY for FEC1: addr 1
Could not get PHY for FEC1: addr 1
Get shared mii bus on ethernet@2188000
PS D:\desktop\6ull> uuu -b emmc_all D:\desktop\6ull\u-boot-emmc-2020.04-r0.imx D:\desktop\6ull\core-image-minimal-imx6ull14x14evk-20210325071354.rootfs.wic.bz2
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.107-0-g9201dde
Success 0 Failure 0
1:11 1/ 1 [=================100%=================] SDP: boot -f D:\desktop\6ull\u-boot-emmc-2020.04-r0.imx
一直卡在这里下不进去。