Dear Sir:
we are using imx6ull for our projects. and face a problem about touch panel.
we have ported the source for a cap touch screen. and I can even get the x/y report value with command "hexdump /dev/input/event1" after click the screen. my lcd is 320X480.
if click left top, it will print
...
0001f10 fc4a 59f6 59e6 0006 0003 0035 0002 0000
0001f20 fc4a 59f6 59e6 0006 0003 0036 002b 0000
...
if click right bottom, it will print
...
0001f90 fcd3 59f6 b731 0001 0003 0035 0115 0000
0001fa0 fcd3 59f6 b731 0001 0003 0036 01df 0000
...
here is the log when I run evtest:
evtest /dev/input/event1
Input driver version is 1.0.1
Input device ID: bus 0x18 vendor 0x0 product 0x0 version 0x0
Input device name: "fts_ts"
Supported events:
Event type 0 (EV_SYN)
Event type 1 (EV_KEY)
Event code 330 (BTN_TOUCH)
Event type 3 (EV_ABS)
Event code 48 (ABS_MT_TOUCH_MAJOR)
Value 0
Min 0
Max 255
Event code 53 (ABS_MT_POSITION_X)
Value 0
Min 0
Max 320
Event code 54 (ABS_MT_POSITION_Y)
Value 0
Min 0
Max 480
Event code 57 (ABS_MT_TRACKING_ID)
Value 0
Min 0
Max 15
Event code 58 (ABS_MT_PRESSURE)
Value 0
Min 0
Max 255
Properties:
Property type 1 (INPUT_PROP_DIRECT)
Testing ... (interrupt to exit)
[FTS][A]P0(301, 2)[p:63,tm:9] DOWN!
Event: time 1509371557.126285, type 3 (EV_ABS), code 57 (ABS_MT_TR[FTS][A]P0(301, 2)[p:63,tm:9] DOWN!
ACKING_ID), value 0
Event: time 1509371557.126285, type 3 (EV_ABS), code 58 (ABS_MT_PR[FTS][A]P0(302, 2)[p:63,tm:9] DOWN!
ESSURE), value 63
Event: time 1509371557.126285, type 3 (EV_ABS), code 48 (ABS_MT_TOUCH_MAJOR), value 9
Event: time 1509371557.1[FTS][A]P0(302, 2)[p:63,tm:9] DOWN!
26285, -------------- SYN_REPORT ------------
Event: time 150937[FTS][A]Points All Up!
1557.129618, type 1 (EV_KEY), code 330 (BTN_TOUCH), value 1
Event: time 1509371557.129618, -------------- SYN_REPORT ------------
Event: time 1509371557.139469, type 3 (EV_ABS), code 57 (ABS_MT_TRACKING_ID), value 0
Event: time 1509371557.139469, type 3 (EV_ABS), code 58 (ABS_MT_PRESSURE), value 63
Event: time 1509371557.139469, type 3 (EV_ABS), code 48 (ABS_MT_TOUCH_MAJOR), value 9
Event: time 1509371557.139469, -------------- SYN_REPORT ------------
Event: time 1509371557.154263, type 3 (EV_ABS), code 57 (ABS_MT_TRACKING_ID), value 0
Event: time 1509371557.154263, type 3 (EV_ABS), code 58 (ABS_MT_PRESSURE), value 63
Event: time 1509371557.154263, type 3 (EV_ABS), code 48 (ABS_MT_TOUCH_MAJOR), value 9
Event: time 1509371557.154263, -------------- SYN_REPORT ------------
Event: time 1509371557.170482, type 3 (EV_ABS), code 57 (ABS_MT_TRACKING_ID), value 0
Event: time 1509371557.170482, type 3 (EV_ABS), code 58 (ABS_MT_PRESSURE), value 63
Event: time 1509371557.170482, type 3 (EV_ABS), code 48 (ABS_MT_TOUCH_MAJOR), value 9
Event: time 1509371557.170482, -------------- SYN_REPORT ------------
Event: time 1509371557.184227, type 1 (EV_KEY), code 330 (BTN_TOUCH), value 0
Event: time 1509371557.184227, ++++++++++++++ SYN_MT_REPORT ++++++++++++
Event: time 1509371557.184227, -------------- SYN_REPORT ------------
but the UI do not response the event.
do you have any idea about this problem?
解決済! 解決策の投稿を見る。
你这里使用的是哪个版本的BSP,Linux还是Android的?
使用的是linux, 去除touch panel multi input相关代码后,touch panel已正常运行。
OK,可以工作了就好
从你上述信息可以看到你底层的驱动是跑起来了,应用层还要添加,你可以可以联系一下你购买屏的厂家要一下该触摸屏的文件添加到应用层就可以了。