hi yuri
In my case, HAB event will be generated if
Blocks = 0x877ff400 0x00000000 0x0008ac00 "u-boot-dtb.imx",\
0x00910000 0x0000002c 0x000001e8 "u-boot-dtb.imx"
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x24 0x42 0x33 0x18 0xc0 0x00
0xca 0x00 0x1c 0x00 0x02 0xc5 0xff 0x00
0x00 0x00 0x0d 0x3c 0x87 0x7f 0xf4 0x00
0x00 0x0a 0x4c 0x00 0x00 0x91 0x00 0x00
0x00 0x00 0x01 0xe8
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_SIGNATURE (0x18)
CTX = HAB_CTX_COMMAND (0xC0)
ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x00
0x00 0x00 0x00 0x20
and HAB event will not be generated if
Blocks = 0x877ff400 0x00000000 0x0008ac00 "u-boot-dtb.imx"
why ???
已解决! 转到解答。
I think i get it.
The csf file of appending dcd blocks is only used as a provisioning program in uuu, the image to be programmed to sd/emmc is still the file w/o dcd.
thank you!
I use uuu tool, because uuu.pdf says to add
0x00910000 0x0000002c 0x000001e8 "u-boot-dtb.imx"
to burn successfully with uuu, if I don’t add it, u-boot-dtb.imx will not be burn. although the burn is successful after add it, but the bootloader cannot be bootup. because HAB event is generated after adding it, which seems very contradictory.
so, how should I set it up specifically so that it can be burned and boot up normal? thanks!
hi yuri
'0x000001e8 'is the exact length of my DCD, Obtained by the following log.
$ cat u-boot-dtb.imx.log
Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 577632 Bytes = 564.09 KiB = 0.55 MiB
Load Address: 877ff420
Entry Point: 87800000
HAB Blocks: 0x877ff400 0x00000000 0x0008ac00
DCD Blocks: 0x00910000 0x0000002c 0x000001e8