imx6ul evk - suspend-on-ram consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul evk - suspend-on-ram consumption

Jump to solution
1,734 Views
giulianofranche
Contributor II


Hi,

we are making some power consumption tests on the imx6ul evaluation board, and we found something which seems a bit odd. When the board enter the "suspend-on-ram" mode, the total consumption of the board goes from 150 mA to 50 mA.

50mA seems quite a lot for this mode. Do we have to modify anything to optimize the power consumption when in deep-sleep mode?

I read the application note AN5170 (http://cache.freescale.com/files/32bit/doc/app_note/AN5170.pdf?pspll=1 ), and the results are very different.

Our image has been made with yocto.

Regards

Labels (1)
0 Kudos
Reply
1 Solution
1,203 Views
igorpadykov
NXP Employee
NXP Employee

available low power modes are provided in

Table 14. Low Power Mode Current and Power Consumption

i.MX6UL Datasheet (rev.0, 8/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf

Best regards

igor

View solution in original post

3 Replies
1,203 Views
igorpadykov
NXP Employee
NXP Employee

Hi giuliano

AN5170 did not measure whole board consumption and it

has many other components which add current. Measured

VDD_SOC_IN, VDD_HIGH_IN, DDR3L and other processor power

domains with all processor modules are disabled.

Peripheral chips power consumption is not included in measurements.

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,203 Views
giulianofranche
Contributor II

Oh, my bad!

Is the hibernation mode available for the imx6ul (suspend-on-disk)? And if not, is it in NXP roadmap for this chip?

0 Kudos
Reply
1,204 Views
igorpadykov
NXP Employee
NXP Employee

available low power modes are provided in

Table 14. Low Power Mode Current and Power Consumption

i.MX6UL Datasheet (rev.0, 8/2015)

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf

Best regards

igor