imx6ul程序烧写

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul程序烧写

1,179 Views
wangqz2010
Contributor I

哪位大侠能够帮帮忙,我在用OTG烧写程序的时候,能够识别OTG,但无法下载程序,不知哪里出了问题?(板子是自己按照开发板画的。)谢谢了!

Tags (1)
0 Kudos
Reply
3 Replies

1,027 Views
lance_lau
Contributor I

你最后解决了没有,怎么解决的?我现在也遇到不能下载的问题。

0 Kudos
Reply

1,027 Views
jimmychan
NXP TechSupport
NXP TechSupport

Are you using MFGtool?

What is the different between your board and evk board?

Have you modify the u-boot and kernel base on the different on your board?

If you are using mfgtool, have you generate a new firmware for your board?

Is there a debug console output from your board? any log message and where is it stopped?

0 Kudos
Reply

1,027 Views
wangqz2010
Contributor I

Hello, thanks for your reply.

Yes I use the MFGtool to download the programs, but my board is a little different from the evk board.

I have not modify the U-boot and kernel, and haven't generate a new firmware for the board.

I am now looking for the reason from the hardware circuit.

BEST REGARDS

0 Kudos
Reply