Hi,
We develop our board on the imx6sx hardware, software is based on the linux kernel 4.9.11.
We use rgb 18bits lcd interface. After linux bring up, the lcd can display the picture stable, but the colour is not right.
To find out the cause, we do the following test. we make the test RGB file which has only one red bit red[7], cat it to /dev/fb0, but the green[0],green[5] also has signal, so the lcd colour looks like yellow.
Our question is
1, Why there is green colour with red colours,while we just send the red[5] colour bit?
The following is our dts set.
&lcdif1
{
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lcd>;
display = <&display0>;
status = "okay";
display0: lcd-display
{
bits-per-pixel = <32>; //
bus-width = <18>;
display-timings
{
......
};
};
};
pinctrl_lcd: lcdgrp
{
fsl,pins =
<
MX6SX_PAD_LCD1_DATA00__LCDIF1_DATA_0 0x4001b0b0
MX6SX_PAD_LCD1_DATA01__LCDIF1_DATA_1 0x4001b0b0
MX6SX_PAD_LCD1_DATA02__LCDIF1_DATA_2 0x4001b0b0
MX6SX_PAD_LCD1_DATA03__LCDIF1_DATA_3 0x4001b0b0
MX6SX_PAD_LCD1_DATA04__LCDIF1_DATA_4 0x4001b0b0
MX6SX_PAD_LCD1_DATA05__LCDIF1_DATA_5 0x4001b0b0
MX6SX_PAD_LCD1_DATA06__LCDIF1_DATA_6 0x4001b0b0
MX6SX_PAD_LCD1_DATA07__LCDIF1_DATA_7 0x4001b0b0
MX6SX_PAD_LCD1_DATA08__LCDIF1_DATA_8 0x4001b0b0
MX6SX_PAD_LCD1_DATA09__LCDIF1_DATA_9 0x4001b0b0
MX6SX_PAD_LCD1_DATA10__LCDIF1_DATA_10 0x4001b0b0
MX6SX_PAD_LCD1_DATA11__LCDIF1_DATA_11 0x4001b0b0
MX6SX_PAD_LCD1_DATA12__LCDIF1_DATA_12 0x4001b0b0
MX6SX_PAD_LCD1_DATA13__LCDIF1_DATA_13 0x4001b0b0
MX6SX_PAD_LCD1_DATA14__LCDIF1_DATA_14 0x4001b0b0
MX6SX_PAD_LCD1_DATA15__LCDIF1_DATA_15 0x4001b0b0
MX6SX_PAD_LCD1_DATA16__LCDIF1_DATA_16 0x4001b0b0
MX6SX_PAD_LCD1_DATA17__LCDIF1_DATA_17 0x4001b0b0
MX6SX_PAD_LCD1_CLK__LCDIF1_CLK 0x4001b0b0
MX6SX_PAD_LCD1_ENABLE__LCDIF1_ENABLE 0x4001b0b0
MX6SX_PAD_LCD1_VSYNC__LCDIF1_VSYNC 0x4001b0b0
MX6SX_PAD_LCD1_HSYNC__LCDIF1_HSYNC 0x4001b0b0
>
}
2, According to the imx6sx reference manual chapter 37, lcdif can convert the rgb888 to rgb666 internal.
so r[0..7] g[0..7] b[0..7] in framebuffer evey pixel will conver to r[0..5],g[0..5],b[0..5] ,then occur on the IOMUX lcd_dat[0..5],lcd_dat[6..11],lcd[12..17], is it right?
we print the lcdif register value like below .Can you help to check.
LCDC_CTRL is 0xa0b21 //18bit databus length, 24bit word length
LCDC_CTRL1 is 0x1070300 //byte packing fmt =0x7
LCDC_CTRL2 is 0x600000
The attachment is our RGB test file
We look forward your help to solve this problem
Hi Joan,
The 18bits is the lcdif hardware interface according to our board design , from pad MX6SX_PAD_LCD1_DATA00__LCDIF1_DATA_0 to pad MX6SX_PAD_LCD1_DATA17__LCDIF1_DATA_17
We have set the bits_per_pixel =32 in the dts file as mentioned before
We find that our Qt software app using the rgb888.
thanks