Hi NXP team,
I found a enet ref clk issue, please help review.
Please check the attachment.
Thanks.
commit 5296da0894582e9695294552544674b4cb883907
Author: Parker.zong <parker.zong@honeywell.com>
Date: Thu Jun 29 17:17:01 2023 +0800
imx6sx: fix enet ref clk issue, please check the comment for details.
diff --git a/arch/arm/boot/dts/imx6sx.dtsi b/arch/arm/boot/dts/imx6sx.dtsi
index 0009216..bf1d48d 100644
--- a/arch/arm/boot/dts/imx6sx.dtsi
+++ b/arch/arm/boot/dts/imx6sx.dtsi
@@ -1076,7 +1076,7 @@
clocks = <&clks IMX6SX_CLK_ENET>,
<&clks IMX6SX_CLK_ENET_AHB>,
<&clks IMX6SX_CLK_ENET_PTP>,
- <&clks IMX6SX_CLK_ENET_REF>,
+ <&clks IMX6SX_CLK_ENET_REF_125M>,
<&clks IMX6SX_CLK_ENET_PTP>;
clock-names = "ipg", "ahb", "ptp",
"enet_clk_ref", "enet_out";
diff --git a/drivers/clk/imx/clk-imx6sx.c b/drivers/clk/imx/clk-imx6sx.c
index d9ff831..5ce2cd9 100644
--- a/drivers/clk/imx/clk-imx6sx.c
+++ b/drivers/clk/imx/clk-imx6sx.c
@@ -231,7 +231,45 @@ static void __init imx6sx_clocks_init(struct device_node *ccm_node)
hws[IMX6SX_CLK_PLL3_USB_OTG] = imx_clk_hw_gate("pll3_usb_otg", "pll3_bypass", base + 0x10, 13);
hws[IMX6SX_CLK_PLL4_AUDIO] = imx_clk_hw_gate("pll4_audio", "pll4_bypass", base + 0x70, 13);
hws[IMX6SX_CLK_PLL5_VIDEO] = imx_clk_hw_gate("pll5_video", "pll5_bypass", base + 0xa0, 13);
- hws[IMX6SX_CLK_PLL6_ENET] = imx_clk_hw_gate("pll6_enet", "pll6_bypass", base + 0xe0, 13);
+ /*
+ * Bit 13 is ENET1_125M_EN, Bit 20 is ENET2_125M_EN
+ * Bit 19 is ENABLE_125M(PCIE), Bit 21 is ENET_25M_REF_EN(PTP)
+ *
+ *
+ * Father-Son Relationship is wrong.
+ * Before:
+ * enet2_ref_125m -> enet2_ref -> pll6_enet -> pll6_bypass
+ * bit 20 bit 13
+ *
+ * pcie_ref_125m -> pcie_ref -> pll6_enet -> pll6_bypass
+ * bit 19 bit 13
+ *
+ * enet_ptp_25m -> enet_ptp_ref -> pll6_enet -> pll6_bypass
+ * bit 21 bit 13
+ *
+ * from here you can see, the bit 13 is father of bit [21,20,19].
+ * so when you enable/disable enet2 or ptp or pcie, also enable/disable enet1.
+ * Actually these bits should be independent.
+ *
+ * After:
+ *
+ * enet2_ref_125m -> enet2_ref -> pll6_enet -> pll6_bypass
+ * bit 20 bit 11
+ *
+ *
+ * pcie_ref_125m -> pcie_ref -> pll6_enet -> pll6_bypass
+ * bit 19 bit 11
+ *
+ * enet_ptp_25m -> enet_ptp_ref -> pll6_enet -> pll6_bypass
+ * bit 21 bit 11
+ *
+ * enet_ref_125m -> enet_ref -> pll6_enet -> pll6_bypass
+ * bit 13 bit 11
+ *
+ * Add IMX6SX_CLK_ENET_REF_125M in imx6sx-clock.h
+ * modification pll6_enet to bit 11, bit 11 is reserved bit, as father of bit [21,20,19,13].
+ */
+ clks[IMX6SX_CLK_PLL6_ENET] = imx_clk_gate("pll6_enet", "pll6_bypass", base + 0xe0, 11);
hws[IMX6SX_CLK_PLL7_USB_HOST] = imx_clk_hw_gate("pll7_usb_host", "pll7_bypass", base + 0x20, 13);
/*
@@ -266,6 +304,7 @@ static void __init imx6sx_clocks_init(struct device_node *ccm_node)
base + 0xe0, 2, 2, 0, clk_enet_ref_table,
&imx_ccm_lock);
hws[IMX6SX_CLK_ENET2_REF_125M] = imx_clk_hw_gate("enet2_ref_125m", "enet2_ref", base + 0xe0, 20);
+ clks[IMX6SX_CLK_ENET_REF_125M] = imx_clk_gate("enet_ref_125m", "enet_ref", base + 0xe0, 13);
hws[IMX6SX_CLK_ENET_PTP_REF] = imx_clk_hw_fixed_factor("enet_ptp_ref", "pll6_enet", 1, 20);
hws[IMX6SX_CLK_ENET_PTP] = imx_clk_hw_gate("enet_ptp_25m", "enet_ptp_ref", base + 0xe0, 21);
diff --git a/include/dt-bindings/clock/imx6sx-clock.h b/include/dt-bindings/clock/imx6sx-clock.h
index 1c64997..d124f56 100644
--- a/include/dt-bindings/clock/imx6sx-clock.h
+++ b/include/dt-bindings/clock/imx6sx-clock.h
@@ -276,6 +276,7 @@
#define IMX6SX_CLK_LVDS2_IN 267
#define IMX6SX_CLK_ANACLK2 268
#define IMX6SX_CLK_MMDC_P1_IPG 269
-#define IMX6SX_CLK_CLK_END 270
+#define IMX6SX_CLK_ENET_REF_125M 270
+#define IMX6SX_CLK_CLK_END 271
#endif /* __DT_BINDINGS_CLOCK_IMX6SX_H */
Hi @ParkerZong,
I hope you are doing well.
Thanks for pointing out the issue.
I will forward the changes provided by you to our BSP maintainers.
does this patch resolve issue?
Thanks & Regards,
Dhruvit Vasavada