Dear all,
i have a wm8988 connected to imx6qp, kernel 4.1.15.
Linux has the wm8988 driver, but machine driver was missing and i am setting up a simple one, based on
similar ASoC machine drivers.
I am actually trying to set imx6qp as i2s master, and codec device as slave.
Card is detected properly and registered, if i try some alsa "speaker-test", i am observing (by scope)
- i2c transfers works fine, tested writing and reading from codec rtegisters
- i2s BCLK, LRframe clock and samples, all driven from cpu
- i see also sysclk, that is sent from CPU CKO output as 24000000,
- i see no output at all from any of the 4 codec analogues outputs. Tried do change mixer settings, aplay, paplay, always
nothing in the outputs.
So my questions actually are:
1) what should be the reasons in selecting the codec mode as i2s master or slave ?
2) Is it ok to be interfaced to the codec with imx6qp as the i2s master ?
3) do you have any knowledge of a similar imx machine driver for a similar codec/scenario ?
Many thanks
angelo
解決済! 解決策の投稿を見る。
Hi Angelo
1. preferable option slave mode, as in that case all clock signals,
frame sync, bit clock, are generated by external codec and allows for more
stable and accurate clocks.
2. ok
3. it may be useful to check
No sound captured with SGTL5000 on i.MX6 in I²S master mode
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor. Still many thanks.
So if i understand correctly, there are
- mclk (master clock)
and
- ssi bitclk (also called system clock (sysclk in linux drivers) and related ssi frame clock, both linked to sample rate.
Hi Angelo
yes, right
Best regards
igor
Hi Igor, thanks for excellent help.
Still a brief question about:
I am assuming sysclk supplied from imx6qp cpu to codec is needed only when codec is the master and it needs to generate bitclock and lrclk from it. Correct ? Or i need to supply still the sysclk (mclk) to the codec even when the codec is just a ssi slave ?
Thanks
angelo
Hi Angelo
port SRCK is used in master and synchronous mode
as network clock (oversampling clock, integer multiple of frame clock).
In other cases its usage is optional.
Best regards
igor
Hi Angelo
1. preferable option slave mode, as in that case all clock signals,
frame sync, bit clock, are generated by external codec and allows for more
stable and accurate clocks.
2. ok
3. it may be useful to check
No sound captured with SGTL5000 on i.MX6 in I²S master mode
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------