Hi lee
I am afraid it does not support, one can add such support using
linux sources (which supports it)
Board Support Packages (5)
i.MX28 Linux 2.6.35 Source Code Files and documentation (REV L2.6.35_1.1.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear igor,
Thanks a lot for your support.
It's a pity that wince BSP does not support the STR function. I'm planning to implement low power consumption.
Kind Regards,