imx6q: u-boot: dual channel LVDS (split mode)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q: u-boot: dual channel LVDS (split mode)

2,083 次查看
pj0585
Contributor III

Hi,

I have a custom hardware based on imx6qsabresd. I'm using dual channel LVDS display (1680x1050), LVDS split mode.

I need to enable UBoot splash image. Any one attempted to enable LVDS split mode in Uboot ?

I'm using ltib's u-boot (2009.08)

Any inputs will be on help?

- Pj

标签 (2)
0 项奖励
回复
3 回复数

890 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Are you using Ubuntu or Android?

Best Regards,

Alejandro

0 项奖励
回复

890 次查看
liyu1
Contributor III

I have such a demand !

                  Thanks! 

0 项奖励
回复

890 次查看
pj0585
Contributor III

Hi Alejandro,

Would it make a difference in U-Boot whether I use Ubuntu or Android?

I'm not using either. I'm using Yocto's linux BSP.

-Pj

0 项奖励
回复