imx6q-sabresd board: No "/dev/ipu" device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6q-sabresd board: No "/dev/ipu" device

跳至解决方案
799 次查看
garyyin
Contributor III

Environment: IMX6Q SabreSD demo board. Yocto, L3.14.28, official.

The .sdcard image is generated by "bitbake fsl-image-qt5". All the code are official, no any change made.

I want to use IPU in the user space.  But no "/dev/ipu" device found.

ls /dev/i*

/dev/i2c-0  /dev/i2c-1  /dev/i2c-2  /dev/initctl

/dev/input:

by-id    event0  event2  event4  event6  event8  mouse0  mouse2

by-path  event1  event3  event5  event7  mice    mouse1

0 项奖励
回复
1 解答
589 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Gary

there are several ipu drivers, seems this one will be as ../dev/mxc_ipu

as described in attached Linux Manual sect.6.2.3 IPU Device Driver.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
590 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Gary

there are several ipu drivers, seems this one will be as ../dev/mxc_ipu

as described in attached Linux Manual sect.6.2.3 IPU Device Driver.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复