Hi
Linux version imx_3.10.53_1.1.0_ga.
I am testing 2 platform Quad and Solo.
They share same design and only the i.MX6 is changed.
While the PCI works fine in the Quad it is not working on the Solo.
dmesg | grep -i pci
imx6q-pcie 1ffc000.pcie: phy link never came up
imx6q-pcie 1ffc000.pcie: failed to initialize host
PCI: CLS 0 bytes, default 64
ehci-pci: EHCI PCI platform driver
Same design with release imx_3.0.35_4.1.0 works fine both Solo and Quad.
Thanks on advance, Bon.
Hi Bon Ton!
Did the new BSP solve your issue? I have the same issue with Linux version imx_3.10.53_1.1.0_ga and imx_3.14.28_1.0.0_ga
Best regards, Ivan.
Hi Bon
one can try new Linux BSP
L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo
Linux Binary Demo Files and Linux BSP Documentation
Size (K): 1479000 Format: gz Rev #: L3.14.28_1.0.0 Modified: 4/10/2015
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------