hi all,
硬件平台:TQ E9_V3开发板
Linux version: 4.1.15
我现在使用i.mx6q的LVDS0接口来驱动9.46inch LVDS接口的LCD,24bit。
现象:静态界面显示色彩不对,播放视频时还会闪屏并出去其他杂色(见图片)
uboot command:
=> printenv mxcfb0
mxcfb0=video=mxcfb0:dev=ldb,1280x240@60,if=RGB24,bpp=32
kernel dts & dtsi
E9-sabresd.dts:
&ldb {
lvds-channel@0 {
crtc = "ipu2-di0";
};
lvds-channel@1 {
crtc = "ipu2-di1";
};
};
e9qdl-sabresd.dtsi:
mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB24";
default_bpp = <32>;
int_clk = <0>;
late_init = <0>;
status = "okay";
};
&ldb {
status = "okay";
dual-mode = <0>;
lvds-channel@0 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";
display-timings {
native-mode = <&timing0>;
timing0: hsd100pxn1 {
clock-frequency = <27700000>;
hactive = <1280>;
vactive = <240>;
hback-porch = <10>;
hfront-porch = <74>;
vback-porch = <82>;
vfront-porch = <16>;
hsync-len = <2>;
vsync-len = <2>;
};
};
图片、屏规书、原理图见附件!
已经在lvds显示异常这道坎上卡了一段时间,求大神解救,多谢!
HI Wigros Sun,
修改ldb的时钟后现象:图片仍然是显示异常,但是给屏的时钟正常了(原先都是38Mhz,现在为正常的27.7Mhz了,道理同该blog:
imx6 适配DLP(864*480)输出 - u013111562的博客 - CSDN博客 )
我修改的是linux dts:
&clks {
fsl,ldb-di0-parent = <&clks IMX6QDL_CLK_PLL5_VIDEO_DIV>;
fsl,ldb-di1-parent = <&clks IMX6QDL_CLK_PLL5_VIDEO_DIV>;
//fsl,ldb-di0-parent = <&clks IMX6QDL_CLK_PLL2_PFD0_352M>;
//fsl,ldb-di1-parent = <&clks IMX6QDL_CLK_PLL2_PFD0_352M>;
}
clk-imx6q.c跟踪:
/*
* Read the LDBID[0/1] parents from the device tree.
* If no entry is found in the device tree, the default
* parent will be set to IMX6QDL_CLK_PLL2_PFD0_352M
*/
static void of_assigned_ldb_sels(struct device_node *node,
int *ldb_di0_sel, int *ldb_di1_sel)
{
struct of_phandle_args clkspec;
int index = 0, rc;
rc = of_parse_phandle_with_args(node, "fsl,ldb-di0-parent",
"#clock-cells", index, &clkspec);
printk("clock-debug ************* rc:%d\n", rc);
if (rc < 0) {
/* skip empty (null) phandles */
if (rc != -ENOENT)
*ldb_di0_sel = IMX6QDL_CLK_PLL2_PFD0_352M;
} else {
*ldb_di0_sel = ldb_di_sel_by_clock_id(clkspec.args[0]);
printk("clock-debug **************** clkspec.args[0]:%d\n", clkspec.args[0]);
if (*ldb_di0_sel == -ENOENT){
printk("clock-debug **************** pll2\n");
*ldb_di0_sel = IMX6QDL_CLK_PLL2_PFD0_352M;
}
...........
}
打印log:
[ 0.000000] clock-debug ************* rc:0
[ 0.000000] clock-debug **************** clkspec.args[0]:195
imx6qdl-clock.h:
...
#define IMX6QDL_CLK_PLL5_POST_DIV 194
#define IMX6QDL_CLK_PLL5_VIDEO_DIV 195
#define IMX6QDL_CLK_EIM_SLOW 196
....
问:如果我设置是正确的,并且不是这个原因导致的显示异常,那么还有什么方法可以排查解决这个问题呢?
--------------------
havd a nice day
CC dason