imx6q Chromium on wayland has no hardware acceleration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q Chromium on wayland has no hardware acceleration

1,272 次查看
BaNe
Contributor IV

Hi,

we have chromium-ozone-wayland_94 running on yocto gatesgarth. It looks like it runs without hardware acceleration for CSS animations, which is making it very sluggish compared to X11 with a older chromium version.

Is there a solution for this issue?

标签 (1)
0 项奖励
回复
2 回复数

1,233 次查看
brian14
NXP TechSupport
NXP TechSupport

Hi @BaNe

I can suggest applying the flags to run chromium with hardware acceleration as follows:

Type on the browser

chrome://flags


Then set the following flags

chrome://flags/#ignore-gpu-blocklist
chrome://flags/#enable-accelerated-video-decode
chrome://flags/#enable-gpu-rasterization

If these flags don't works please help me using the following command on chromium.

chrome://gpu

This command will help me to analyze the issue with the gpu acceleration.

Have a great day!

0 项奖励
回复

1,216 次查看
BaNe
Contributor IV

Hi @brian14 

I tried the parameters and this is what about gpu shows:

 

Graphics Feature Status
Canvas: Hardware accelerated
Canvas out-of-process rasterization: Disabled
Direct Rendering Display Compositor: Disabled
Compositing: Software only. Hardware acceleration disabled
Multiple Raster Threads: Enabled
OpenGL: Enabled
Rasterization: Hardware accelerated on all pages
Raw Draw: Disabled
Skia Renderer: Enabled
Video Decode: Software only. Hardware acceleration disabled
Video Encode: Software only. Hardware acceleration disabled
Vulkan: Disabled
WebGL: Hardware accelerated but at reduced performance
WebGL2: Hardware accelerated but at reduced performance
Driver Bug Workarounds
clear_uniforms_before_first_program_use
enable_webgl_timer_query_extensions
exit_on_context_lost
disabled_extension_GL_KHR_blend_equation_advanced
disabled_extension_GL_KHR_blend_equation_advanced_coherent
disabled_extension_GL_MESA_framebuffer_flip_y
Problems Detected
Accelerated video encode has been disabled, either via blocklist, about:flags or the command line.
Disabled Features: video_encode
Accelerated video decode has been disabled, either via blocklist, about:flags or the command line.
Disabled Features: video_decode
Gpu compositing has been disabled, either via blocklist, about:flags or the command line. The browser will fall back to software compositing and hardware acceleration will be unavailable.
Disabled Features: gpu_compositing
Clear uniforms before first program use on all platforms: 124764, 349137
Applied Workarounds: clear_uniforms_before_first_program_use
Disable KHR_blend_equation_advanced until cc shaders are updated: 661715
Applied Workarounds: disable(GL_KHR_blend_equation_advanced), disable(GL_KHR_blend_equation_advanced_coherent)
Expose WebGL's disjoint_timer_query extensions on platforms with site isolation: 808744, 870491
Applied Workarounds: enable_webgl_timer_query_extensions
Some drivers can't recover after OUT_OF_MEM and context lost: 893177
Applied Workarounds: exit_on_context_lost
Disable GL_MESA_framebuffer_flip_y for desktop GL: 964010
Applied Workarounds: disable(GL_MESA_framebuffer_flip_y)
Version Information
Data exported	2023-06-28T08:57:12.299Z
Chrome version	Chrome/101.0.4951.54
Operating system	Linux 5.4.84-botox+g789b344baa2c
Software rendering list URL	https://chromium.googlesource.com/chromium/src/+/67da1aeb32cedd27634ca6634fb79cbd85d3f0ab/gpu/config/software_rendering_list.json
Driver bug list URL	https://chromium.googlesource.com/chromium/src/+/67da1aeb32cedd27634ca6634fb79cbd85d3f0ab/gpu/config/gpu_driver_bug_list.json
ANGLE commit id	unknown hash
2D graphics backend	Skia/101 e72c4af441c8c842236343f3c218bf4a349df9be
Command Line	/usr/bin/chromium --ozone-platform=wayland --disable-features=VizDisplayCompositor --in-process-gpu --disable-features=VizDisplayCompositor --enable-crashpad --gpu-preferences=WAAAAAAAAAAoAAAIAAAAAAAAAAAAAAAAAABgAAAAAAA4AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAACAAAAAAAAAAIAAAAAAAAAAAAAAAAAAAAAgAAAAAAAAACAAAAAAAAAAIAAAAAAAAAA== --in-process-gpu --no-sandbox --ozone-platform=wayland --enable-crashpad --flag-switches-begin --enable-gpu-rasterization --ignore-gpu-blocklist --flag-switches-end --gpu-preferences=WAAAAAAAAAAoAAAoAAAAAAAAAAAAAAAAAABgAAAAAAA4AAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAAACAAAAAAAAAAIAAAAAAAAAAAAAAAAAAAAAgAAAAAAAAACAAAAAAAAAAIAAAAAAAAAA==
Driver Information
Initialization time	216
In-process GPU	true
Passthrough Command Decoder	false
Sandboxed	false
GPU0	VENDOR= 0x0000, DEVICE=0x0000
Optimus	false
AMD switchable	false
Driver vendor	
Driver version	
GPU CUDA compute capability major version	0
Pixel shader version	
Vertex shader version	
Max. MSAA samples	
Machine model name	
Machine model version	
GL_VENDOR	
GL_RENDERER	
GL_VERSION	
GL_EXTENSIONS	
Disabled Extensions	GL_KHR_blend_equation_advanced GL_KHR_blend_equation_advanced_coherent GL_MESA_framebuffer_flip_y
Disabled WebGL Extensions	
Window system binding vendor	
Window system binding version	
Window system binding extensions	
Interfaces exposed by the Wayland compositor	wl_compositor:4 wl_subcompositor:1 wp_viewporter:1 zxdg_output_manager_v1:2 wp_presentation:1 zwp_alpha_compositing_v1:1 zwp_relative_pointer_manager_v1:1 zwp_pointer_constraints_v1:1 zwp_input_timestamps_manager_v1:1 wl_data_device_manager:3 wl_shm:1 weston_touch_calibration:1 wl_viv:1 zwp_linux_explicit_synchronization_v1:2 wl_seat:7 wl_output:3 zwp_input_panel_v1:1 zwp_input_method_v1:1 zwp_text_input_manager_v1:1 xdg_wm_base:1 zxdg_shell_v6:1 wl_shell:1 weston_desktop_shell:1 weston_screenshooter:1 zwp_linux_dmabuf_v1:3 wl_drm:2
Ozone platform	wayland
Direct rendering version	unknown
Reset notification strategy	0x0000
GPU process crash count	0
gfx::BufferFormats supported for allocation and texturing	R_8: not supported, R_16: not supported, RG_88: not supported, RG_1616: not supported, BGR_565: not supported, RGBA_4444: not supported, RGBX_8888: not supported, RGBA_8888: not supported, BGRX_8888: not supported, BGRA_1010102: not supported, RGBA_1010102: not supported, BGRA_8888: not supported, RGBA_F16: not supported, YVU_420: not supported, YUV_420_BIPLANAR: not supported, P010: not supported
Compositor Information
Tile Update Mode	One-copy
Partial Raster	Enabled
GpuMemoryBuffers Status
R_8	Software only
R_16	Software only
RG_88	Software only
RG_1616	Software only
BGR_565	Software only
RGBA_4444	Software only
RGBX_8888	Software only
RGBA_8888	Software only
BGRX_8888	Software only
BGRA_1010102	Software only
RGBA_1010102	Software only
BGRA_8888	Software only
RGBA_F16	Software only
YVU_420	Software only
YUV_420_BIPLANAR	Software only
P010	Software only
Display(s) Information
Info	Display[18] bounds=[0,0 1280x800], workarea=[0,0 1280x800], scale=1, rotation=0, panel_rotation=0 external.
Color space (all)	{primaries:BT709, transfer:SRGB, matrix:RGB, range:FULL}
Buffer format (all)	RGBA_8888
SDR white level in nits	100
HDR relative maximum luminance	1
Bits per color component	8
Bits per pixel	24
Video Acceleration Information
Encoding	
Vulkan Information
Device Performance Information

 

chromium puts into the console

 

[3762:3782:0628/085115.075446:ERROR:file_path_watcher_linux.cc(321)] inotify_init() failed: Too many open files (24)
[     1] Failed EGL API GetProcAddress: eglBindWaylandDisplayWL !
[     2] Failed EGL API GetProcAddress: eglUnbindWaylandDisplayWL !
[     3] Failed EGL API GetProcAddress: eglQueryWaylandBufferWL !
[     4] Failed EGL API GetProcAddress: eglUpdateWaylandBufferWL !
[     5] Failed EGL API GetProcAddress: eglSwapBuffersWithDamageEXT !
[     6] Failed EGL API GetProcAddress: eglPatchID !
[     7] Failed ES_Common API GetProcAddress: forward_glActiveTexture !
[     8] Failed ES_Common API GetProcAddress: forward_glBindBuffer !
[     9] Failed ES_Common API GetProcAddress: forward_glBindTexture !
[    10] Failed ES_Common API GetProcAddress: forward_glBlendFunc !
[    11] Failed ES_Common API GetProcAddress: forward_glBufferData !
[    12] Failed ES_Common API GetProcAddress: forward_glBufferSubData !
[    13] Failed ES_Common API GetProcAddress: forward_glClear !
[    14] Failed ES_Common API GetProcAddress: forward_glClearColor !
[    15] Failed ES_Common API GetProcAddress: forward_glClearDepthf !
[    16] Failed ES_Common API GetProcAddress: forward_glClearStencil !
[    17] Failed ES_Common API GetProcAddress: forward_glColorMask !
[    18] Failed ES_Common API GetProcAddress: forward_glCompressedTexImage2D !
[    19] Failed ES_Common API GetProcAddress: forward_glCompressedTexSubImage2D !
[    20] Failed ES_Common API GetProcAddress: forward_glCopyTexImage2D !
[    21] Failed ES_Common API GetProcAddress: forward_glCopyTexSubImage2D !
[    22] Failed ES_Common API GetProcAddress: forward_glCullFace !
[    23] Failed ES_Common API GetProcAddress: forward_glDeleteBuffers !
[    24] Failed ES_Common API GetProcAddress: forward_glDeleteTextures !
[    25] Failed ES_Common API GetProcAddress: forward_glDepthFunc !
[    26] Failed ES_Common API GetProcAddress: forward_glDepthMask !
[    27] Failed ES_Common API GetProcAddress: forward_glDepthRangef !
[    28] Failed ES_Common API GetProcAddress: forward_glDisable !
[    29] Failed ES_Common API GetProcAddress: forward_glDrawArrays !
[    30] Failed ES_Common API GetProcAddress: forward_glDrawElements !
[    31] Failed ES_Common API GetProcAddress: forward_glEnable !
[    32] Failed ES_Common API GetProcAddress: forward_glFinish !
[    33] Failed ES_Common API GetProcAddress: forward_glFlush !
[    34] Failed ES_Common API GetProcAddress: forward_glFrontFace !
[    35] Failed ES_Common API GetProcAddress: forward_glGenBuffers !
[    36] Failed ES_Common API GetProcAddress: forward_glGenTextures !
[    37] Failed ES_Common API GetProcAddress: forward_glGetBooleanv !
[    38] Failed ES_Common API GetProcAddress: forward_glGetBufferParameteriv !
[    39] Failed ES_Common API GetProcAddress: forward_glGetError !
[    40] Failed ES_Common API GetProcAddress: forward_glGetFloatv !
[    41] Failed ES_Common API GetProcAddress: forward_glGetIntegerv !
[    42] Failed ES_Common API GetProcAddress: forward_glGetPointerv !
[    43] Failed ES_Common API GetProcAddress: forward_glGetString !
[    44] Failed ES_Common API GetProcAddress: forward_glGetTexParameterfv !
[    45] Failed ES_Common API GetProcAddress: forward_glGetTexParameteriv !
[    46] Failed ES_Common API GetProcAddress: forward_glHint !
[    47] Failed ES_Common API GetProcAddress: forward_glIsBuffer !
[    48] Failed ES_Common API GetProcAddress: forward_glIsEnabled !
[    49] Failed ES_Common API GetProcAddress: forward_glIsTexture !
[    50] Failed ES_Common API GetProcAddress: forward_glLineWidth !
[    51] Failed ES_Common API GetProcAddress: forward_glPixelStorei !
[    52] Failed ES_Common API GetProcAddress: forward_glPolygonOffset !
[    53] Failed ES_Common API GetProcAddress: forward_glReadPixels !
[    54] Failed ES_Common API GetProcAddress: forward_glSampleCoverage !
[    55] Failed ES_Common API GetProcAddress: forward_glScissor !
[    56] Failed ES_Common API GetProcAddress: forward_glStencilFunc !
[    57] Failed ES_Common API GetProcAddress: forward_glStencilMask !
[    58] Failed ES_Common API GetProcAddress: forward_glStencilOp !
[    59] Failed ES_Common API GetProcAddress: forward_glTexImage2D !
[    60] Failed ES_Common API GetProcAddress: forward_glTexParameterf !
[    61] Failed ES_Common API GetProcAddress: forward_glTexParameterfv !
[    62] Failed ES_Common API GetProcAddress: forward_glTexParameteri !
[    63] Failed ES_Common API GetProcAddress: forward_glTexParameteriv !
[    64] Failed ES_Common API GetProcAddress: forward_glTexSubImage2D !
[    65] Failed ES_Common API GetProcAddress: forward_glViewport !
[    66] Failed ES_Common API GetProcAddress: forward_glMapBufferOES !
[    67] Failed ES_Common API GetProcAddress: forward_glUnmapBufferOES !
[    68] Failed ES_Common API GetProcAddress: forward_glEGLImageTargetTexture2DOES !
[    69] Failed ES_Common API GetProcAddress: forward_glEGLImageTargetRenderbufferStorageOES !
[    70] Failed ES_Common API GetProcAddress: forward_glMultiDrawArraysEXT !
[    71] Failed ES_Common API GetProcAddress: forward_glMultiDrawElementsEXT !
[    72] Failed ES_Common API GetProcAddress: forward_glTexDirectVIV !
[    73] Failed ES_Common API GetProcAddress: forward_glTexDirectInvalidateVIV !
[    74] Failed ES_Common API GetProcAddress: forward_glTexDirectVIVMap !
[    75] Failed ES_Common API GetProcAddress: forward_glTexDirectTiledMapVIV !
[    76] Failed GLES32 API GetProcAddress: glMultiDrawArraysEXT !
[    77] Failed GLES32 API GetProcAddress: glMultiDrawElementsEXT !
[    78] Failed GLES32 API GetProcAddress: glTexDirectVIV !
[    79] Failed GLES32 API GetProcAddress: glTexDirectInvalidateVIV !
[    80] Failed GLES32 API GetProcAddress: glTexDirectVIVMap !
[    81] Failed GLES32 API GetProcAddress: glTexDirectTiledMapVIV !
[    82] Failed GLES32 API GetProcAddress: glGetTexImage !
[    83] Failed ES Common GLES2X API GetProcAddress: glMultiDrawArraysEXT !
[3762:3793:0628/085115.206123:ERROR:gl_context_egl.cc(352)] eglCreateContext failed with error EGL_SUCCESS
[3762:3793:0628/085115.206811:ERROR:gl_context_egl.cc(352)] eglCreateContext failed with error EGL_SUCCESS
[3762:3793:0628/085115.206887:ERROR:gpu_info_collector.cc(93)] gl::init::CreateGLContext failed
[3762:3793:0628/085115.206938:ERROR:gpu_info_collector.cc(365)] Could not create context for info collection.
[3762:3793:0628/085115.208457:ERROR:gl_context_egl.cc(352)] eglCreateContext failed with error EGL_SUCCESS
[3762:3793:0628/085115.208537:ERROR:gpu_info_collector.cc(93)] gl::init::CreateGLContext failed
[3762:3793:0628/085115.208587:ERROR:gpu_info_collector.cc(365)] Could not create context for info collection.
[3798:3816:0628/085115.347612:ERROR:file_path_watcher_linux.cc(321)] inotify_init() failed: Too many open files (24)
[3762:3762:0628/085115.385733:ERROR:cursor_loader.cc(116)] Failed to load a platform cursor of type kNull
[3762:3793:0628/085115.709612:ERROR:gl_context_egl.cc(352)] eglCreateContext failed with error EGL_SUCCESS
[3762:3793:0628/085115.709728:ERROR:gpu_channel_manager.cc(831)] ContextResult::kFatalFailure: Failed to create shared context for virtualization.
[3762:3793:0628/085115.709780:ERROR:shared_image_stub.cc(537)] SharedImageStub: unable to create context
[3762:3793:0628/085115.709848:ERROR:gpu_channel.cc(572)] GpuChannel: Failed to create SharedImageStub
[3762:3793:0628/085115.710069:ERROR:gl_context_egl.cc(352)] eglCreateContext failed with error EGL_SUCCESS
[3762:3793:0628/085115.710136:ERROR:gpu_channel_manager.cc(831)] ContextResult::kFatalFailure: Failed to create shared context for virtualization.
[3762:3793:0628/085115.710182:ERROR:shared_image_stub.cc(537)] SharedImageStub: unable to create context
[3762:3793:0628/085115.710247:ERROR:gpu_channel.cc(572)] GpuChannel: Failed to create SharedImageStub
[3762:3793:0628/085115.710449:ERROR:gl_context_egl.cc(352)] eglCreateContext failed with error EGL_SUCCESS
[3762:3793:0628/085115.710528:ERROR:gpu_channel_manager.cc(831)] ContextResult::kFatalFailure: Failed to create shared context for virtualization.
[3762:3793:0628/085115.710581:ERROR:shared_image_stub.cc(537)] SharedImageStub: unable to create context
[3762:3793:0628/085115.710652:ERROR:gpu_channel.cc(572)] GpuChannel: Failed to create SharedImageStub
[3762:3851:0628/085115.715385:ERROR:object_proxy.cc(623)] Failed to call method: org.freedesktop.DBus.Properties.Get: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: The name org.freedesktop.UPower was not provided by any .service files
[3762:3851:0628/085115.716929:ERROR:object_proxy.cc(623)] Failed to call method: org.freedesktop.UPower.GetDisplayDevice: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: The name org.freedesktop.UPower was not provided by any .service files
[3762:3851:0628/085115.718359:ERROR:object_proxy.cc(623)] Failed to call method: org.freedesktop.UPower.EnumerateDevices: object_path= /org/freedesktop/UPower: org.freedesktop.DBus.Error.ServiceUnknown: The name org.freedesktop.UPower was not provided by any .service files
[3762:3793:0628/085115.726681:ERROR:gl_context_egl.cc(352)] eglCreateContext failed with error EGL_SUCCESS
[3762:3793:0628/085115.726790:ERROR:gpu_channel_manager.cc(831)] ContextResult::kFatalFailure: Failed to create shared context for virtualization.
[3762:3793:0628/085115.726850:ERROR:shared_image_stub.cc(537)] SharedImageStub: unable to create context
[3762:3793:0628/085115.726930:ERROR:gpu_channel.cc(572)] GpuChannel: Failed to create SharedImageStub

 

 

0 项奖励
回复