Hello support team,
Configuration:
MACHINE=imx6dlsabresd DISTRO=fsl-imx-wayland source ./imx-setup-release.sh -b fsl_image_test
bitbake fsl-image-machine-test
snippet from Yocto project user guide Rev. LF5.15.32_2.0.0, 12 July 2022
fsl-image-machine-test An FSL Community i.MX core image with console
environment - no GUI interface. meta-freescale-distro
snippet end
Query:
i am building the image with the above configuration
For the above image, Yocto splash screen with GUI comes first then the terminal will appear or directly the terminal will be opened.
i am looking for the image to be build without Splash screen only with the terminal opens directly
please confirm
Thanks
Solved! Go to Solution.
Do i need to enable SSH manually in the configuration file for core-image-minimal. please confirm
CORE_IMAGE_EXTRA_INSTALL += "openssh"
PACKAGE_EXCLUDE += " packagegroup-core-ssh-dropbear"
CORE_IMAGE_EXTRA_INSTALL += "packagegroup-core-ssh-openssh"
Hello shankovai,
You need build the core-image-mininal.
Regards