imx6dq local alpha blending in platform sdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6dq local alpha blending in platform sdk

506 Views
ajaykumar
Contributor I

We need to use bare metal SDK and we found that it does not have any example for IPU local alpha blending. The Firmware guide says channel 31 should be enabled for local alpha blending but there is no information how to do it. Can you please help us to enable local alpha blending in imx6 Platform SDK.

Thanks

Labels (4)
0 Kudos
1 Reply

348 Views
igorpadykov
NXP Employee
NXP Employee

HI ajay

one can refer to linux alpha_ex2 example

ipu-examples release notes - v0.1

unfortunately bare metal SDK is not supported as linux BSPs with

updates and patches. If you have urgent need it may be recommended

to apply to  Freescale Professional Services to develop it

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_PROFESSIONAL

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos