imx6ULL WDOG1_ANY signal = same as imx6SoloX WDOG1_ANY?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6ULL WDOG1_ANY signal = same as imx6SoloX WDOG1_ANY?

跳至解决方案
933 次查看
r_veens
Contributor III

Hey,

We are looking at the watchdogs of the imx6ull and we find that the first instance (WDOG1) has an extra signal named WDOG1_ANY.

The imx6ULL RM does not say anything about this external signal.

 

This post mentions that the signal is the logical AND of all the WDOG_B signals of all watchdog instances:

https://community.nxp.com/t5/i-MX-Processors/About-WDOG1-ANY-signal-of-i-MX6SoloX/td-p/459008 

 

My question is, is this true as well for the imx6ull?

 

I see that the IMX6soloX RM has since been updated:

r_veens_0-1611339647807.png

 

But this is not the case for the IMX6ULL:

r_veens_1-1611339679142.png

 

Would someone be able to clarify this? Thanks in advance.

标签 (2)
0 项奖励
回复
1 解答
925 次查看
igorpadykov
NXP Employee
NXP Employee

Hi r_veens

 

yes this is also true for the imx6ull.

 

Best regards
igor

 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
926 次查看
igorpadykov
NXP Employee
NXP Employee

Hi r_veens

 

yes this is also true for the imx6ull.

 

Best regards
igor

 

 

0 项奖励
回复