imx6S USDHC4 MTFC4GLDDQ-4M IT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6S USDHC4 MTFC4GLDDQ-4M IT

2,728 Views
ken_sallings1
Contributor III

We created a custom board with a Micron eMMC; however, we are having trouble communicating with the eMMC.  We have loaded u-boot via jtag; however, the eMMC never seems to respond to command 0 and u-boot hangs when trying to communicate with the device.  On SDHC2 we have an SD card connected and it never hangs when communicating with SD2.  Is this eMMC incompatible with the i.mx6?

0 Kudos
11 Replies

2,235 Views
ken_sallings1
Contributor III

We wired an SDCard to SD2 on our board.  We also changed the boot strap resistors to boot from SD2.  When I did this, we can boot the board from SD2 and we can talk to the eMMC on SD4.  I have a feeling that errata ERR007926 bit us.  We are getting the latest processor put on the board and I will post an answer to this after we solve it.

0 Kudos

2,236 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ken

recommended to check schematic (attached Sabre SD schematic,

eMMC on p.5) and eMMC signals with oscilloscope.

Linux Guide sect.4.4.1.2 Using eMMC4.4 on SDHC4 shows how to

work with eMMC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,236 Views
ken_sallings1
Contributor III

eMMC_Schem.png

Above is the schematic for our design with this chip.  Here is what we have previously tried.

We are using u-boot-2015-10

I load u-boot via jtag.  Then u-boot hangs waiting for register uSDHCx_INT_STATUS bit CTOE or bit CC to be set.  It is never set.  When I look at the clock it is running at around 370kHz.  The CMD line is stuck low.  Any ideas would be greatly appreciated.

0 Kudos

2,236 Views
igorpadykov
NXP Employee
NXP Employee

suggest to check if SION bit is set for i.MX6 uSDHC pads.

~igor

0 Kudos

2,236 Views
ken_sallings1
Contributor III

The SION bit is set for the CMD line.  For all of the others it is cleared.  Below is a list of all of the registers and their values, right before the USDHC4 hangs.

020e0338:  0x00000000

020e033c:  0x00000010

020e0340:  0x00000001

020e0344:  0x00000001

020e0348:  0x00000001

020e034c:  0x00000001

020e0350:  0x00000001

020e0354:  0x00000001

020e0358:  0x00000001

020e035c:  0x00000001

020e0720:  0x00017059

020e0724:  0x00017059

020e0728:  0x00017059

020e072c:  0x00017059

020e0730:  0x00017059

020e0734:  0x00017059

020e0738:  0x00017059

020e073c:  0x00017059

020e0740:  0x00017059

020e0744:  0x00017059

0 Kudos

2,234 Views
igorpadykov
NXP Employee
NXP Employee

probably it makes sense to test it with bare metal SDK, you can request

it from : Re: Where is the i.MX6 Platform SDK?

0 Kudos

2,237 Views
ken_sallings1
Contributor III

Should it be set or cleared?

0 Kudos

2,239 Views
ThomasG1z
Contributor III

I have the exact same device on a custom imx6s board as well and it works fine. What happens in linux when you boot from the SD, is it detected? 100% sure the config in both linux and u-boot is set correctly?

0 Kudos

2,239 Views
ken_sallings1
Contributor III

What is the part number on your imx6S?

0 Kudos

2,236 Views
ThomasG1z
Contributor III

Currently we use the MCIMX6S5EVM10ACR. Also used the B version previously.

0 Kudos

2,236 Views
ken_sallings1
Contributor III

Our current board is the B part.  I have switched booting from eMMC to booting from SPI-NOR.  Then I finish booting from MMC.  u-boot-spl goes in the SPI NOR.  And the rest of u-boot goes in the eMMC along with the kernel.  I am 99% confident that revision 1.3 of the chip will solve the eMMC boot; however, it can't just be the C part, it has to be the C part with a particular mask.  Ordering that part has been a problem.  I am not sure how we will get that part.  I would like to cut the SPI-NOR out of the BOM.

0 Kudos