imx6Q ONOFF信号与PMIC_ON_REQ的开关与时序关系的说明文档

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6Q ONOFF信号与PMIC_ON_REQ的开关与时序关系的说明文档

5,738 Views
bratzhang
Contributor II

您好:

请问有没有imx6Q ONOFF信号与PMIC_ON_REQ的开关与时序关系的说明文档,可能我看文档不太细,并未在RM里面找到时序说明。

们在测试中,使用3.0V纽扣电池供给PMIC_SNVS,而PMIC_ON_REQ信号电平不为低, 短按开机键PMIC_ON_REQ没有变化;而开机后长拉5s ONOFF可以使PMIC_ON_REQ由高电平变为低电平,与官方文档符合。但是我们不需要用户在开机的时候每次需要复杂的操作才能开机,多谢。

Labels (1)
0 Kudos
2 Replies

3,649 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Brat,

     开机和关机,你可以不做成你描述的方式。ONOFF引脚在内部有100K电阻拉高,可以保证上电就可以启动CPU的,PMIC_ON_REQ引脚是一个 Opendrain引脚,但是内部有100K拉高,如果你不用PMIC电源芯片,那么悬空就可以了。

      所以,基本上开机是这样的(假设你使用PMIC):4.2V电一给到PMIC,PMIC就会输出并使CPU启动。因此要希望开机和关机变得简单,你只要控制4.2v上电与否,就可以了。

Regards.

weidong

0 Kudos

3,649 Views
bratzhang
Contributor II

Hi Weidong:

      您好!目前我们需求是使用物理按键来做开关机控制,物理按键分别连接到CPU SNVS的ONOFF与一个GPIO input,那么在无法使用IMX6 PMIC_ON_REQ的情况下,如何使用开关逻辑电路实现对电源的使能进行控制?

     目前测试PMIC_ON_REQ在ONOFF low level 5秒之后会拉低,符合规格书。是否750ms~5s的逻辑有问题? RevC参考设计中的FDC6321电路是否完成验证测试,因为从mos管开关逻辑来看没有问题。我们这一边还没有验证。

     此外,请问有没有用分立元件供电IMX6Q的参考电路?谢谢。

0 Kudos