imx6DL How to make the input std PAL signal full screen display by a/d tp2825

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6DL How to make the input std PAL signal full screen display by a/d tp2825

1,825件の閲覧回数
liangfeng_0824
Contributor I

I want to full screen display now,But unsuccessfulHow to set up software?

my software settings are as follows

   p->if_type = V4L2_IF_TYPE_BT656; /* This is the only possibility. */
    p->u.bt656.mode = V4L2_IF_TYPE_BT656_MODE_NOBT_8BIT;
    p->u.bt656.nobt_hs_inv = 0;  
    p->u.bt656.bt_sync_correct = 1;     //use gated mode

    p->u.bt656.clock_curr = 37000000;

As the pixel after conversion through tp2825 is  960*624,The input of tp2825 A/D is STD CVBS PAL。

Use  param below:

Parameters are modified below,The image is displayed as follows:

   {            /*! (B, G, H, I, N) PAL */
     .v4l2_id = V4L2_STD_PAL,
     .name = "PAL",
     .raw_width = 960,    
     .raw_height = 624,  
     .active_width = 960, 
     .active_height = 312,
     .active_top = 0,
     .active_left = 0,
     },

    22.jpg

Parameters are modified below,The image is displayed as follows:

{            /*! (B, G, H, I, N) PAL */
     .v4l2_id = V4L2_STD_PAL,
     .name = "PAL",
     .raw_width = 960,    
     .raw_height = 624,  
     .active_width = 960,
     .active_height = 624-16
     .active_top = 0,
     .active_left = 0,
     },

33.jpg

 

11.bmp

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,183件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi feng

please try interlaced-mode-capture patch on
https://community.nxp.com/docs/DOC-158531

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,183件の閲覧回数
liangfeng_0824
Contributor I

hi  igorpadykov

I am using i.MX6DualLite  android6.0.1  now, Please specify that I should use that

The project is more urgent, need your help,tks!

22.bmp

0 件の賞賛
返信

1,183件の閲覧回数
liangfeng_0824
Contributor I
Which patch should I use?
0 件の賞賛
返信

1,183件の閲覧回数
xiaojunye
Contributor I

Hi fengliang,

         Do your problems solved? Now i also use tp2825 video decoding. The tp2825 input is 480i cvbs with NTSC,the output is 8 bit bt656. But the video is scrolling . Do you have good problems?

0 件の賞賛
返信

1,183件の閲覧回数
liangfeng_0824
Contributor I

I now use the i.MX6DualLite  android6.0.1  kernel software version is :

44.bmp

Please confirm which patch I should use now?

0 件の賞賛
返信