imx6 u-boot ltib nothing on minicom

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 u-boot ltib nothing on minicom

跳至解决方案
1,019 次查看
alexandredel
Contributor I

Hello everybody

I am trying to flash a u-boot on my sabrelite board, however, when i use imx loader with the u boot created by ltib, nothing appear on minicom. When i try with the u-boot.bin, it succeed but there is nothing on the minicom's prompt, and when i try with the u-boot, it says:

unknown load address

HAB security state: development mode (0x56787856)

And of course, there is nothing on the prompt.

Do you have an idea how to fix this?

Thanks

Alexandre

标签 (1)
0 项奖励
1 解答
624 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

actually sabrelite board uses own bootloaders and special methods for flashing them.

Please refer to excellent help resource below and post issue if this will not help

on boundary devices forum

http://eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite+SPI+Flash+Recovery

http://boundarydevices.com/community/

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
625 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

actually sabrelite board uses own bootloaders and special methods for flashing them.

Please refer to excellent help resource below and post issue if this will not help

on boundary devices forum

http://eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite+SPI+Flash+Recovery

http://boundarydevices.com/community/

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励